Debian build fail ( tflite_ethosu_delegate] Error 2) in flexbuild v24.12 and imx8mpevk.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debian build fail ( tflite_ethosu_delegate] Error 2) in flexbuild v24.12 and imx8mpevk.

1,106 次查看
charleshuang
Senior Contributor II

Hi NXP,

We are following the NXP Release Debian 2024/12/30 version as per the official documentation:

https://docs.nxp.com/bundle/UG10155/page/topics/building_an_image_in_flexbuild.html

We followed the standard procedure described in the "Most used examples with automated build" section and run the command:

blb -m imx8mpevk

We understand that this process may involve building a Debian Docker image with ML features.

Could you confirm whether it is possible to successfully compile the Docker image using this method?
If not, could you provide the correct SOP (Standard Operating Procedure) for building it?

We have strictly followed NXP's official SOP, but we are encountering issues.
Please let us know the correct steps to complete the build successfully.

Thanks,

 

 

build_fail.jpg

0 项奖励
回复
6 回复数

1,090 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport
0 项奖励
回复

1,071 次查看
charleshuang
Senior Contributor II

Hi @Zhiming_Liu 

In the thread, you say : "Please use Ubunut22.04 as host environment."

So, do you mean we shouldn't use the Docker environment?

Please provide the correct the SOP.  Thanks.

0 项奖励
回复

1,065 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

If you need ML feature, you need use docker under Ubuntu22.04.

Ubuntu22.04----->without ML

Ubuntu22.04+Debian12 docker------>ML/non-ML

Best Regards,
Zhiming

0 项奖励
回复

1,039 次查看
charleshuang
Senior Contributor II

Hi @Zhiming_Liu 

We tested on two different Ubuntu 22.04 PCs, both using the Debian 12 Docker image provided by NXP.

However, the compilation still failed.

Do you have any suggestions?"

0 项奖励
回复

1,003 次查看
charleshuang
Senior Contributor II

Hi @Zhiming_Liu 

Thanks for your help.

We change use the Azure VM (Cloud vm), the result is pass.

标记 (1)
0 项奖励
回复

1,067 次查看
charleshuang
Senior Contributor II

Hi @Zhiming_Liu 

May I compile without ML?
Do you have any advice?

Thanks.

标记 (1)
0 项奖励
回复