Data transfer from OTG to USB-A in imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Data transfer from OTG to USB-A in imx6

1,909 次查看
avenkatramani
Contributor III

Hi 

imx6 board having OTG for MFGTOOL (production)   and USB-A host.

is it possible to communicate with OTG and USB-A in imx6? (with two different boards)

is any configuration changed needed in kernel.

kindly advice how to achieve with imx6 

标签 (2)
标记 (1)
0 项奖励
回复
3 回复数

1,717 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Arunkumar

i.MX6 uses otg port in device mode, mfg tool usage is described in presentation

AMF-ACC-T1652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,717 次查看
avenkatramani
Contributor III

thanks for the replay.

In my application i need to use the OTG to transfer data to the USB host connected imx.

kindly share if any document available

0 项奖励
回复

1,717 次查看
igorpadykov
NXP Employee
NXP Employee

one can look at usb unit tests

doc\mxc_usb_test\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor

0 项奖励
回复