Data throughput

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Data throughput

890 次查看
eishishibusawa
Contributor III

Dear Sir

 

Customer want to know the throughput when using i.MX6Dual.

There is no data processing in the CPU.

Please consider that there is only data forwarding.

 

Q1.

From PCIe to SATA(SSD).

Is it possible to achieve the throughput more than 100 MB/s?

 

Q2.

How much is the throughput from G-Ethernet to SATA(SSD)?

 

Please let me know if you have any information.

 

Best Regards,

Eishi SHIBUSAWA

标签 (2)
0 项奖励
回复
1 回复

796 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Elshi

1. seems yes, based on throughput data provided on

https://community.nxp.com/docs/DOC-95014 

2. sorry, such data is not available, such hardware were not tested.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复