DY1212W-4856 LVDS Panel with i.MX 93 EVK on top of out of box demo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DY1212W-4856 LVDS Panel with i.MX 93 EVK on top of out of box demo

Jump to solution
1,877 Views
JACK_CHA
Contributor IV

Hi NXP 

About DY1212W-4856 - NXP Semiconductors

 

A customer purchased an iMX 93 EVK, and received a report that the LVDS Panel purchased together does not turn on.
Please answer if the image downloaded at the factory with Out of Box Demo is also outputting LVDS.
I'm asking because I think it takes a long time to download a new version of Linux 6.1.22_2.0.0 and try to make an image and test it.

If any of DISPLAY interface is not activated by default of Out of box demo or New SDK release, 

Please let us know how to activate LVDS output along with i.MX 93 EVK.

Thanks.

Regards, 

ADAM

0 Kudos
1 Solution
1,760 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @JACK_CHA 

I hope you are doing well.

default device tree imx93-11x11-evk.dtb does not support LVDS display.
 
The customer can change the device tree blob to imx93-11x11-evk-boe-wxga-lvds-panel in u-boot cmd as below for LVDS display.
=> setenv fdtfile imx93-11x11-evk-boe-wxga-lvds-panel.dtb
=> saveenv
=> reset
 
I hope it helps!
 
Thanks & Regards,
Sanket Parekh

View solution in original post

16 Replies
1,657 Views
jmaja
Contributor I

Any luck on this?  I tried both the pre-built and a microSD - wic and my LVDS still not working. Do you have any image for how to connect the connector at the back?

just wanted to be sure I did not mess up my connection.

Thanks,

Joe

0 Kudos
1,638 Views
JACK_CHA
Contributor IV

Hi

My customer identified it works fine with the uboot script below.

=> setenv fdtfile imx93-11x11-evk-boe-wxga-lvds-panel.dtb
=> saveenv
=> reset
 
Thanks.
Regards, 
ADAM
0 Kudos
1,818 Views
JACK_CHA
Contributor IV

Hi 

Subject changed. adding DY1212W-4856 LVDS panel part number.

Please let us know if DY1212W-4856 could be activated on top of LINUX SDK 6.1.1_1.0.0 or 6.1.22_2.0.0. 

A customer bought this LVDS module from nxp.com. But it does not work with Out of Box Pre-built image programmed on i.MX 93 EVK.

Thanks.

Regards, 

ADAM

0 Kudos
1,761 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @JACK_CHA 

I hope you are doing well.

default device tree imx93-11x11-evk.dtb does not support LVDS display.
 
The customer can change the device tree blob to imx93-11x11-evk-boe-wxga-lvds-panel in u-boot cmd as below for LVDS display.
=> setenv fdtfile imx93-11x11-evk-boe-wxga-lvds-panel.dtb
=> saveenv
=> reset
 
I hope it helps!
 
Thanks & Regards,
Sanket Parekh
1,529 Views
bitspirate
Contributor III

Hi

I just wanted to confirm that this solution worked for me.

What seems to not be working is the touchpanel (the ability to use the DY1212W-4856 as touchpanel.

Is this supposed to work out of the box? (I do see the screen with the terminal to the left and the time to the right)

Regards

0 Kudos
1,393 Views
bitspirate
Contributor III

Hi

This.

Has anyone figured out how to enable the touch functionality?

Regards

0 Kudos
1,268 Views
mharlan
Contributor II

The panel I received had the touch panel pins in the harness pinned incorrectly.

i2C SDA and SCL were flipped and the reset and ground pins were flipped.

Once I corrected the pinout, the touch panel is working as expected for me.

 

I followed the test point labels on the Touch flex PCB vs the EVK pinout and found the mistake.

 

0 Kudos
1,199 Views
bitspirate
Contributor III

Could you share the touch flex PCB pinout? Cannot find it

0 Kudos
1,179 Views
mharlan
Contributor II

The only place I was able to find the pinout for the the TP Flex was on the flex itself, hiding under the masking tape used to hold it down.

 

J702 (LVDS) on the reference board is in the published schematics.  Check continuity to find the errors.

 

As I mentioned, out of the 6 pins for the TP, 4 were wrong.  Once corrected the TP controller is recognized and worked as expected.

 

 

1,075 Views
bitspirate
Contributor III

Hi

This is the solution!

Same problem, 4 pins were swapped

Tags (1)
0 Kudos
1,341 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @bitspirate,

I hope you are doing well.

"Has anyone figured out how to enable the touch functionality?"
->Please mention the revision of the EVK.

Thanks & Regards,
Sanket Parekh

0 Kudos
1,336 Views
bitspirate
Contributor III

Hi @Sanket_Parekh 
On top were he processor is there is written TDA9695
On the bottom I have these indicators:
- TDA9695
- 700-51961 Rev A1
- SCH-51961 Rev B2
The bar code indicates: TR23120373
Thanks, it would be great to hear from you.

0 Kudos
1,198 Views
bitspirate
Contributor III

Revision is B2.

0 Kudos
1,826 Views
JACK_CHA
Contributor IV

Hi Sanket.

I confirmed the prebuilt-binary programmed into eMMC works fine with MIPI-DSI output.

And also the latest 6.1.22 based image works with SD card too.

However the customer still could not see the linux screen from their LVDS screen. The backlight was not turned on at all.

Can you check if JP701 BLT Connector is also needed to connect with LVDS? 

ADAM_ArrowFAE_0-1691149113501.png

 

I could not see the JP101 connected with LVDS from below figure.

ADAM_ArrowFAE_1-1691149168498.png

 

Regards, 

ADAM

 

0 Kudos
1,835 Views
JACK_CHA
Contributor IV

Hi Sanket.

Thanks for your kind reply.

 

As Customer tried the same setup as decribed at Quick start guide. 

LVDS does not turn on at all.

Is there any other instruction to output LVDS  with out-of-box image?

 

ADAM_ArrowFAE_0-1691132456041.png

ADAM_ArrowFAE_1-1691132564290.png

 

 

0 Kudos
1,845 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @JACK_CHA,

I hope you are doing well.

The pre-built image should work actually as described in the quick start guide of the i.MX93.

Please refer to this document.
https://www.nxp.com/webapp/Download?colCode=IMX93EVKQSG

->One can find detailed information about SETTING UP THE SYSTEM(step 3 Connect LVDS panel Display) in the GETTING STARTED Section.

I hope it will be helpful.

Thanks & Regards,
Sanket Parekh

0 Kudos