Hi,
We are planning to use i.MX 6ULL processor in our project. When we are checking about the DVFS feature in this processor we got confused while referring the datasheet of the processor and the dtsi file for the processor.
In the datasheet of the processor they had given like for 792 MHz the VDD_SOC_IN voltage is 1.325 - 1.5 V and for 528 MHz and below the VDD_SOC_IN voltage is 1.275 - 1.5 V. But in the dtsi file they had given like for both 792 and 528 MHz the voltage value to be 1.175V.
So our doubt is why there is a difference between the voltage values between the datasheet and dtsi file, and what voltage values must be updated in the dtsi file for using DVFS feature?
Also why there are 2 tables in the dtsi file?
Solved! Go to Solution.
Hi Ranjith
NXP BSPs are developed for reference boards, so dtsi file is for i.MX6ULL EVK with
processor MCIMX6Y2DVM05AA (528 MHz) - i.MX 6ULL Applications Processors for Consumer Products
voltages are defined in Table 10. Operating Ranges. Other parts, like Industrial grade or with
higher operating frequencies may require other dts "operating-points" parameters.
Please check with datasheet of used processor.
Also there are some patches on link i.MX Software and Development Tools | NXP
>Also why there are 2 tables in the dtsi file?
because both VDD_ARM_CAP and VDD_SOC_CAP can be changed depending
on operating frequency.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ranjith
NXP BSPs are developed for reference boards, so dtsi file is for i.MX6ULL EVK with
processor MCIMX6Y2DVM05AA (528 MHz) - i.MX 6ULL Applications Processors for Consumer Products
voltages are defined in Table 10. Operating Ranges. Other parts, like Industrial grade or with
higher operating frequencies may require other dts "operating-points" parameters.
Please check with datasheet of used processor.
Also there are some patches on link i.MX Software and Development Tools | NXP
>Also why there are 2 tables in the dtsi file?
because both VDD_ARM_CAP and VDD_SOC_CAP can be changed depending
on operating frequency.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks for your reply.
We are using Industrial grade processor and in the datasheet it is given as it supports 528 and 792 MHz, so is it okay to include those two frequencies only in the dtsi file or including other frequencies also won't cause problem?
Thanks,
Ranjith
Hi Ranjith
yes only frequencies given in datasheet should be included in dts.
Best regards
igor
Hi Igor,
Thanks for your help. We will include 528 and 792 MHz in the dtsi file as per the datasheet of i.MX 6ULL Industrial grade processor.
Thanks
Ranjith