DVFS feature on IMX6ULL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DVFS feature on IMX6ULL

2,055件の閲覧回数
fabio_poiatti
Contributor III

Hi

in our custom board we use the IMX6ULL with DVFS pin connected as evalution board.

Now ... I have some doubts about the functionality.

I addedd the DVFS block in the DTS file as the EVK and added also the power management in menu config kernel

And now?

How is possible for the kernel to lead correctly DFVFS pin?

What I have to do to have the DVFS funzctionality working?

Thanks

Fabio

0 件の賞賛
返信
2 返答(返信)

2,004件の閲覧回数
art
NXP Employee
NXP Employee

Do you mean the PMIC_STBY_REQ pin of the processor? If so, please note that this pin is only functional when the system goes to the power saving mode (OS goes to sleep).

For the information on how to put the system to the power saving mode and then resume it, please refer to the Section 6.1 "Suspend and resume" of the attached document.

Best Regards,
Artur

0 件の賞賛
返信

2,004件の閲覧回数
fabio_poiatti
Contributor III

thanks

Fabio

0 件の賞賛
返信