Hi all
According to the table 1 of AN5170, it shows voltage levels in some case of ARM freq.
For example, VDDARM is 0.925V when frequency is 198MHz.
Also according to the table 2 of AN4715, it shows voltage levels in some case of ARM freq, too.
For example, VDDARM is 0.95V when frequency is 396MHz.
I have a question about those .
Which drivers control those VDDARM's voltage ?
Ko-hey
解決済! 解決策の投稿を見る。
imx6q.dtsi
22 #size-cells = <0>;
23
24 cpu0: cpu@0 {
25 compatible = "arm,cortex-a9";
26 device_type = "cpu";
27 reg = <0>;
28 next-level-cache = <&L2>;
29 operating-points = <
30 /* kHz uV */
31 1200000 1275000
32 996000 1250000
33 852000 1250000
34 792000 1175000
35 396000 975000
36 >;
37 fsl,soc-operating-points = <
38 /* ARM kHz SOC-PU uV */
39 1200000 1275000
40 996000 1250000
41 852000 1250000
42 792000 1175000
43 396000 1175000
44 >;
"~/imx_builder/rel_imx_3.14.52_1.1.0_ga/kernel_imx/arch/arm/boot/dts/imx6q.dtsi" 267L,
In the each one of the BSP release, contains a document i.MX_6_Linux_Reference_Manual.pdf.
Hi BiyongSUN
Sorry for late reply.
I checked some source that is shown in i.MX_6_Linux_Reference_Manual.pdf.
However, I can't find a value of voltage setting.
Could you tell me that which source file is included about it ?
Ko-hey
imx6q.dtsi
22 #size-cells = <0>;
23
24 cpu0: cpu@0 {
25 compatible = "arm,cortex-a9";
26 device_type = "cpu";
27 reg = <0>;
28 next-level-cache = <&L2>;
29 operating-points = <
30 /* kHz uV */
31 1200000 1275000
32 996000 1250000
33 852000 1250000
34 792000 1175000
35 396000 975000
36 >;
37 fsl,soc-operating-points = <
38 /* ARM kHz SOC-PU uV */
39 1200000 1275000
40 996000 1250000
41 852000 1250000
42 792000 1175000
43 396000 1175000
44 >;
"~/imx_builder/rel_imx_3.14.52_1.1.0_ga/kernel_imx/arch/arm/boot/dts/imx6q.dtsi" 267L,
Hi Biyong Sun
I checked it and found in other kernel version.
L3.14.28 /tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/linux-libc-headers/3.14-r0/linux-3.14/arch/arm/boot/dts
L3.14.38 /build-6ul-x11/tmp/work-shared/imx6qsabresd/kernel-source/arch/arm/boot/dts
Thank you for your cooperation.
Ko-hey