DTSI file format for imx6sl

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DTSI file format for imx6sl

Jump to solution
2,368 Views
eugenephua
Contributor III

Hello there, i was looking at the imx6sl.dtsi file at linux-2.6-imx.git - Freescale i.MX Linux Tree and saw the uart1 and uart4 entry. How does the fsl,pins entry come about? An example taken from the code is: MX6SL_PAD_SD1_DAT4__UART4_RX_DATA 0x1b0b1


How does the 0x1b0b1 comes about? Thanks!

Labels (2)
1 Solution
1,984 Views
Yuri
NXP Employee
NXP Employee

The line “MX6SL_PAD_SD1_DAT4__UART4_RX_DATA 0x1b0b1”
means : i.MX6 SL SD1_DATA4 will be configured as UART4_RX_DATA (ALT4)
and value of the Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_SD1_DATA4)
will be init as 0x1b0b1.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,985 Views
Yuri
NXP Employee
NXP Employee

The line “MX6SL_PAD_SD1_DAT4__UART4_RX_DATA 0x1b0b1”
means : i.MX6 SL SD1_DATA4 will be configured as UART4_RX_DATA (ALT4)
and value of the Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_SD1_DATA4)
will be init as 0x1b0b1.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,984 Views
eugenephua
Contributor III

Hi Yuri, thanks for the great explanation. One last thing is how do i map the values 0x1b0b1 to

CONFIG bits definition:
PAD_CTL_LVE (1 << 22)
PAD_CTL_HYS (1 << 16)
PAD_CTL_PUS_100K_DOWN (0 << 14)
PAD_CTL_PUS_47K_UP (1 << 14)
PAD_CTL_PUS_100K_UP (2 << 14)
PAD_CTL_PUS_22K_UP (3 << 14)
PAD_CTL_PUE (1 << 13)
PAD_CTL_PKE (1 << 12)
PAD_CTL_ODE (1 << 11)
PAD_CTL_SPEED_LOW (1 << 6)
PAD_CTL_SPEED_MED (2 << 6)
PAD_CTL_SPEED_HIGH (3 << 6)
PAD_CTL_DSE_DISABLE (0 << 3)
PAD_CTL_DSE_240ohm (1 << 3)
PAD_CTL_DSE_120ohm (2 << 3)
PAD_CTL_DSE_80ohm (3 << 3)
PAD_CTL_DSE_60ohm (4 << 3)
PAD_CTL_DSE_48ohm (5 << 3)
PAD_CTL_DSE_40ohm (6 << 3)
PAD_CTL_DSE_34ohm (7 << 3)
PAD_CTL_SRE_FAST (1 << 0)

PAD_CTL_SRE_SLOW (0 << 0)

thanks!

0 Kudos
Reply
1,984 Views
Yuri
NXP Employee
NXP Employee

  According to section 30.4.335 (Pad Control Register)  of the i.MX6 SL Reference
Manual,

IOMUXC_SW_PAD_CTL_PAD_SD1_DATA4 = 0x1b0b1


means :

PAD_CTL_SRE_FAST (1 << 0)

PAD_CTL_DSE_40ohm (6 << 3)

PAD_CTL_SPEED_MED (2 << 6)

PAD_CTL_PUE (1 << 13)

PAD_CTL_PKE (1 << 12)

PAD_CTL_PUS_100K_UP (2 << 14)

PAD_CTL_HYS (1 << 16)

Regards,

Yuri.