DT028ATFT LCD MODULE based on ILI9341 driver chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DT028ATFT LCD MODULE based on ILI9341 driver chip

702 Views
PramodKumar
Contributor IV

hi

plz tell me how to initialize the DT028ATFT lcd on imx233

plz give me source code for  RGB interface on imx233 board becouse i don't have source code for initalize the this lcd on imx233

Thanks&regards

pramod kumar

Labels (3)
0 Kudos
1 Reply

340 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pramod

I am not aware of such driver, however

for RGB connection one can look at below link

(as i.MX23 has similar LCDIF module) and reuse existing

i.MX23 EVK driver in drivers/video/mxs/lcd_43wvf1g.c

Re: i.MX28 LCD ILI9341V porting

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos