DRAM_ADDRxx pad control of i.MX6Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DRAM_ADDRxx pad control of i.MX6Solo

Jump to solution
1,046 Views
宗標廖
Contributor V

Hello Community

About registers IOMUXC_SW_PAD_CTL_PAD_DRAM_ADDRxx of i.MX6, I have some questions.

1)DSE needs to be configured and ODT does not need to be configured(just set ODT to 000), is it right?

2)If 1) is not right, how should ODT be configured?

Best Regards

ZongbiaoLiao

Labels (1)
0 Kudos
Reply
1 Solution
948 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following : ODT setting for i.MX6UL 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

View solution in original post

0 Kudos
Reply
2 Replies
949 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following : ODT setting for i.MX6UL 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply
948 Views
宗標廖
Contributor V

Hi Yuri

Thank you for your answer!

ZongbiaoLiao

0 Kudos
Reply