DOSE IMX.8m and Imx.8mm has the EIM interface like in IMX.6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DOSE IMX.8m and Imx.8mm has the EIM interface like in IMX.6?

519 Views
karl_deng
Contributor I

DATASHEET IMX.8M 和8MM module list里都有 EIM 出现,但是在后面章节 IO 中并没有找到相关IO,请问

到底有没有呢? 如果没有,module list 中又出现 很容易误导人啊

Labels (1)
0 Kudos
1 Reply

467 Views
igorpadykov
NXP Employee
NXP Employee

Hi Carl

these procesors have not EIM interface.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos