DIR_BT_DIS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DIR_BT_DIS?

1,449 Views
bw1
Contributor IV

Does the DIR_BT_DIS apply to all external memory boot instances (e.g. FlexSPI NOR) or just enhanced Direct Memory Access?  In other words if it is set, then booting from any external memory is disabled? 

The reference manual doesn't provide much detail about this efuse. It refers to "NXP reserved modes" in one section, but also in the SRC_SBMR2 section has:  "DIR_BT_DIS shows the state of the DIR_BT_DIS fuse. See Chapter 5, Fusemap for additional information on this fuse."  Chapter 5 is "Enhanced Direct Memory Access".

0 Kudos
2 Replies

1,282 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Really the mentioned fuse is "enable/disable Freescale Reserved Modes" and not 

"Direct Boot from External Memory". Direct Boot from External Memory is not used

in i.MX6.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

939 Views
kanimozhi_t
Contributor V

@Yuri thanks for the info! What do you mean by  "enable/disable Freescale Reserved Modes"? Could you provide us more context?

Is "DIR_BT_DIS" applicable to i.MX 6SX processor? (we can't find it in the security reference manual)

0 Kudos