DESIGN iMAX6Q PROCESSOR BASED CUSTOM HARDWARE WITH SEPARATE MEMORY CARD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DESIGN iMAX6Q PROCESSOR BASED CUSTOM HARDWARE WITH SEPARATE MEMORY CARD

639 Views
peteramond
Contributor V

DEAR ALL,

WE CAN FIND MANY DEVELOPMENT BOARDS WHICH ARE BASED ON IMAX6Q PROCESSOR LIKE SABRE LITE, NITROGEN 6, SABRE SD, REX AND ETC. ALL OF THEM USE ON BOARD RAM WITH THEIR HARDWARE DESIGN.

DO YOU HAVE ANY EXAMPLE BOARD WITH MEMORY CARD SLOT ? (WHICH WE CAN PLUG AND UNPLUG MEMORY LIKE A CARD)

ANY SUGGESTION TO REDUCE THE SPACE OF THE PCB LAYOUT ? CAN WE USE FLEX PCB IN BETWEEN MEMORY AND PROCESSOR LAYOUT AREA ?

REGARDS,

PETER.

0 Kudos
1 Reply

422 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

>DO YOU HAVE ANY EXAMPLE BOARD WITH MEMORY CARD SLOT ? (WHICH WE CAN PLUG AND >UNPLUG MEMORY LIKE A CARD)

sorry NXP does not provide such reference design

 

ANY SUGGESTION TO REDUCE THE SPACE OF THE PCB LAYOUT ? CAN WE USE FLEX PCB IN BETWEEN MEMORY AND PROCESSOR LAYOUT AREA ?

in general flex pcb also can be used, for layout please follow guidelines described in

i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos