DEK reuse in CST for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEK reuse in CST for i.MX6

Jump to solution
1,303 Views
michalhojsik
Contributor II

Hi.

I am working on encrypted boot on i.MX6 and I would like to use one DEK in several builds. The goal is to keep the same DEK and do not let CST to generate new DEK each time it runs.

In the "backend code" of the Code Signing Toll (CST), file $(CST-HOME)/code/back_end/src/adapt_layer_openssl.c, function "gen_auth_encrypted_data(...)" has arguments  "key_file" and "reuse_dek". However, there is not obvious way to provide this key_file name to the function.

After couple of tries I found out that the CST version 2.3.3 has a "hidden" command line argument "--dek" that (as I believe) should allow me to specify the DEK file name. Indeed, if I ran the tool with --dek argument, for example

../linux64/cst --o u-boot_csf.bin --i u-boot.csf --dek dek.bin

it does not complain and even prints some warning about key-reuse. However, then the tool crashes with "Segmentation fault (core dumped)".

So the question is: How can I reuse the DEK between CST runs?

Regards,

Michal

Labels (1)
1 Solution
1,070 Views
tomwang
Contributor II

I try CST3.1.0 it can support dek.bin reuse.

cst -d -i cst.txt -o cst.bin

BR.

Tom.

View solution in original post

4 Replies
1,071 Views
tomwang
Contributor II

I try CST3.1.0 it can support dek.bin reuse.

cst -d -i cst.txt -o cst.bin

BR.

Tom.

1,070 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Current CST implementations do not support the needed (DEK reuse) feature.

Please accept apologies for this inconvenience.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,070 Views
michalhojsik
Contributor II

Hi Jury.

Does NXP have plans to support this feature in a future CST releases?

If yes, can you share CST release plan?

Regards,

Michal

0 Kudos
1,070 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I do not have such information.

You may try to create request to get more details.

https://community.nxp.com/docs/DOC-329745 

Regards,

Yuri.

0 Kudos