DDR3L interface with Fly-by topology

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3L interface with Fly-by topology

3,792 Views
mrudangshelat
Contributor IV

Hi,

I have made board with DDR3L design using 32bit, I have done routing with Fly-by topology but I have not added bus termination resistor in my design.
Can you please tell me what will be the effect on the board and how can I solve this issue?
Regards,
Mrudang
Labels (2)
7 Replies

3,137 Views
art
NXP Employee
NXP Employee

Typically, if no more than 4 memory chips is used and the PCB traces impedance is matched to 50 Ohm for single-ended signals and to 100 Ohm for differential pairs, the VTT termination is not required even when using the fly-by topology. In other case, the only way to fix the possible DDR bus issues is to redesign the PCB layout to add the VTT termination circuit.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,137 Views
mrudangshelat
Contributor IV

Hi Artur,

Thanks for the reply.

I have used 2  x DDR3L - 16 bit (Total system 32 bit) with Fly-by topology. And both are on TOP side only.

Please see attached image for your reference.

It means that my design will work without any issue though I don't kept bus termination resistors.

The fabrication of oard is done and it is in assembly preocess.

Regards,

Mrudang

2 x DDR3L to iMX6D.bmp

0 Kudos
Reply

3,137 Views
art
NXP Employee
NXP Employee

Most likely, it will work without any issue.

Best Regards,

Artur

3,137 Views
mrudangshelat
Contributor IV

Hi Artur,

Thanks for reply.

Parallally I am working on similar board which has iMX6Q with 4 x DDR3L (MT41K512M16HA-125:A) (Total density = 4GB).

  1. Can you please suggest me which is the right topology to rout DDR3L?
  2. Since I am using 4 DDR3L do I need to provide bus termination resistor support?

Provide me your valuable answer.

Regards,

Mrudang

0 Kudos
Reply

3,137 Views
art
NXP Employee
NXP Employee

1. The preferred topology for 4 memory chips with i.MX6 series processors is T-type. Please follow the design of the i.MX6 SABRE SD board.

2. No VTT termination is required in case of 4 memory chips with T topology routing.

Best Regards,

Artur

0 Kudos
Reply

3,137 Views
rahulsoni
Contributor II

Hi Artur

I'm  designing a board which can contain i.MX6 Quad, i.MX6 duallite and i.MX6 Solo in the same PCB. 

When using Quad, we'll put 4 x DDR3L (MT41K512M16HA-125:A) (Total density = 4GB).

When using duallite we'll put  2 x DDR3L (MT41K512M16HA-125:A) (Total density = 2GB). making other 2 DDR3L no mount.

When using Solo we'll put  1 x DDR3L (MT41K512M16HA-125:A) (Total density = 1GB). making other 3 DDR3L no mount.

My doubt is that if I go with balanced T topology, will there be noise due to the stubs which will be there in the absence of 3 DDR3L RAMs (As in i.MX6 Solo configuration, the PCB remains same and only 1 DDR is populated)?

Or should I go with Flyby topology keeping all four RAMs on top layer? 

0 Kudos
Reply

3,137 Views
art
NXP Employee
NXP Employee

You are right in that populating only one DDR chip on balanced T-topology bus may affect the signal integrity due to signal reflection on unused trace stubs. In this case, actually, the Fly-by topology seems to be more appropriate.

Best Regards,

Artur