DDR3 size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,757件の閲覧回数
Arm7
Contributor II

In the i.MX6 SOLO is there a way to read the size of the chip DDR3 ?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,749件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello!

You can do it in U-boot with the command bdinfo.

That command will show to you information about of the board, including the DRAM size.

Look for "size" under of DRAM bank section.

 

I hope this can help to you.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,750件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello!

You can do it in U-boot with the command bdinfo.

That command will show to you information about of the board, including the DRAM size.

Look for "size" under of DRAM bank section.

 

I hope this can help to you.

0 件の賞賛
返信
2,741件の閲覧回数
Arm7
Contributor II
Hello @Manuel_Salas, Thanks for your answer,
So, I have another questions, same topic:
Is there a way to automatically detect different types of DDR3 in SPL/u-boot ?
0 件の賞賛
返信
2,719件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Arm7 , 

Unfortunately, in U-boot that is not possible, but for IMX6 Solo the supported interfaces are 16/32-bit DDR3-800, and LV-DDR3-800.

Best regards!

0 件の賞賛
返信