DDR3 layout for i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR3 layout for i.MX6

697件の閲覧回数
ramansubramania
Contributor I

NXP recommendation for the layout of the DDR3 with
a two chip solution is to use a balanced T for the clock, address, and command
lines, which is how it is implemented  on the Saber board.  In
the NXP layout recommendations, you list the lengths of each of the
groups.  In particular, you list the max length of the clock traces to be
no greater than 2.25 inches.  In a balanced T configuration, does this
consider the total length of the T (both branches), or is it the distance from
the iMX6 to a DDR3 pad?

The reason customer is  asking is that they  conform to the latter
but not the former.  Any thoughts/advice/suggestions?

ラベル(1)
0 件の賞賛
返信
1 返信

397件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Raman

max length assumes distance from the iMX6 to a DDR3 pad.

In general if design does not conform this, recommended to perform

ibis modelling for finding optimal layout.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信