We are working on imx6 solo board. Due to hardware space constraint, the data lines between DDR3 controller (IS43TR16256B-125KBL) and imx6 solo processor (MCIMX6S5EVM10AD) are swapped.
Data bit D11 from DDR3 controller is connected to Data bit D14 of imx6 solo processor and Data bit D14 from DDR3 controller is connected to Data bit D11 of imx6 solo processor.
For the lines swapped, what changes are we supposed to do for DDR3 control registers ?
or any changes in Board support package?
Hi @SUV,
I hope you are doing well.
There is no requirement for any specific control register changes.
For more information, please refer to the link given below:
https://community.nxp.com/t5/i-MX-Processors/ddr3-data-lines-swapped-imx6sl/m-p/324402
Thanks & Regards,
Ritesh M Patel