Hi,
I am trying to find a 512MB Micron DDR3 chip for i.MX6SL. I can only find MT41K256M16TW -093 and -107 in current market. The NXP compatibility chart is suggesting MT41K256M16HA -125: E, which is difference speed grade.
And the i.MX6SL datasheet only mentioned DDR3-800. So I don't know if I can use -093 and -107 for it. Please suggest a part number for me..
Also, I am only using one DDR3 chip for the MCU. The ACC signals are pin to pin connection. Do I still need to terminate them to Vtt? Thanks.
Solved! Go to Solution.
Hi Yan
different speed grades are also supported, one can use -093 and -107 grades
even i.MX6SL datasheet only mentioned DDR3-800.
For schematic connections one can look at i.MX6Q/DL Sabre SD board design files
as i.MX6SL has similar MMDC module:
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yan
different speed grades are also supported, one can use -093 and -107 grades
even i.MX6SL datasheet only mentioned DDR3-800.
For schematic connections one can look at i.MX6Q/DL Sabre SD board design files
as i.MX6SL has similar MMDC module:
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------