DDR3 calibration i.MX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3 calibration i.MX6ULL

1,161 Views
ban45
Contributor III
Hi I have adjusted DDR3 with iMX6 Solo. Is it the same method for i.MX6ULL? Can I use DDR Stress Test Tool V3.00? Where can I find the i.MX6ULL script file? Change the following registers from the log file. Is there any change from Solo? MMDC_MPWLDECTRL0 ch0 MMDC_MPWLDECTRL1 ch0 MMDC_MPWLDECTRL0 ch1 MMDC_MPWLDECTRL1 ch1 MPDGCTRL0 PHY0 MPDGCTRL1 PHY0 MPDGCTRL0 PHY1 MPDGCTRL1 PHY1 MPRDDLCTL PHY0 MPRDDLCTL PHY1 MPWRDLCTL PHY0 MPWRDLCTL PHY1 best regard
0 Kudos
3 Replies

1,154 Views
Yuri
NXP Employee
NXP Employee
0 Kudos

1,138 Views
ban45
Contributor III

Hi

I downloaded I.MX6ULL_DDR3_Script_Aid_V0.01.xlsx, but the Memory type was up to DDR3-1600 and DDR3-1866 was missing. Is it okay to enter the Memory type as DDR3-1600?

best regard.

0 Kudos

1,130 Views
Yuri
NXP Employee
NXP Employee

@ban45 
Hello,

  i.MX 6ULL MMDC supports clock rate of up to 400 MHz, so memory timings
should be based on DDR3-800 specs.

Regards,
Yuri.

0 Kudos