DDR3 Swapping data lines and yocto configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DDR3 Swapping data lines and yocto configuration

跳至解决方案
1,947 次查看
juanalbertogonz
Contributor II

Hi,  

we are working with a custom board, that implemented data lines swapping,  the note says target DDR IC register read value must be transposed according to the data line swapping.

Where should I look to set this transpose value into the yocto configuration? Or how this transpose  is configured?

0 项奖励
回复
1 解答
1,931 次查看
jamesbone
NXP TechSupport
NXP TechSupport

There is no need for additional mapping or software reconfiguration, as

it is done automatically. Bit swapping is described in sect.3.5.1 Swapping data lines IMX6DQ6SDLHDG

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,924 次查看
igorpadykov
NXP Employee
NXP Employee

Hi juanalbertogonz

 

regarding " target DDR IC register read value must be transposed according to the data line swapping." -

this is needed for reading MR registers of ddr part. For DDR3(L) memories such reading is not

used. So this may be ignored for DDR3(L).

 

Best regards
igor

0 项奖励
回复
1,908 次查看
juanalbertogonz
Contributor II

Thanks for the answer

0 项奖励
回复
1,932 次查看
jamesbone
NXP TechSupport
NXP TechSupport

There is no need for additional mapping or software reconfiguration, as

it is done automatically. Bit swapping is described in sect.3.5.1 Swapping data lines IMX6DQ6SDLHDG

 

0 项奖励
回复
1,909 次查看
juanalbertogonz
Contributor II

Thanks for the answer

0 项奖励
回复