DDR3 Script aid question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DDR3 Script aid question

1,054 次查看
preeteshrathod
Contributor I

I would like to point out two things related to DDR3 script aid for IMX6 series.

   1. The current versions of DDR3 scipt aid for all IMX6 series processor does not provide separate Drive strength setting for IMX6 and DDR memory which as per my understanding should be provided. Otherwise we need to change it manually when we are using different strength at IMX6 and at Memory. 

  2. Dynamic ODT is default enabled by this script aid but I think it is better to have option to enable or disable dynamic ODT. Nowhere in the script aid it is mentioned that dynamic ODT is enabled. I think this should be clearly indicated.

Let me know what IMX6 team thinks on above two points. 

标签 (1)
0 项奖励
回复
1 回复

848 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  I think it makes sense to apply directly to authors via DDR Stress test discussion

in Community.

i.MX6/7 DDR Stress Test Tool V2.52 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 项奖励
回复