DDR3 Register settings for MCIMX6SX-SDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3 Register settings for MCIMX6SX-SDB

790 Views
Richard1z
Contributor II

We cannot use the DDR3 Script Tool on our new IMX6SX board - as the tool does not support this processor as yet.

Our Memory design is similar to the MCIMX6SX-SDB.

Can anyone supply me with the DDR3 settings used on the MCIMX6SX-SDB platform please ?

(With this I will then make the necessary calibration modifications).

R

Labels (1)
0 Kudos
2 Replies

465 Views
igorpadykov
NXP Employee
NXP Employee

HI Richard

one can look at dcd settings in

uboot-imx-imx_v2014.04_3.14.28_1.0.0_ga/board/freescale/mx6sxsabresd

uboot-imx.git - Freescale i.MX u-boot Tree

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

465 Views
gusarambula
NXP TechSupport
NXP TechSupport

Just to add to the conversation, the Script Aid for i.MX6SX is now released on the following links:

i.MX6SX DDR3 Register Programming Aid

https://community.freescale.com/docs/DOC-105969

i.MX6SX LPDDR2 Register Programming Aid
https://community.freescale.com/docs/DOC-105970

0 Kudos