DDR3 FLY BY TOPOLOGY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,763件の閲覧回数
raghavendraanja
Contributor II

IMX6 processor with fly by topology routing meets the timing wrt to the JEDEC specification but the voltage levels are less than 1V where it is suppose to be 1.5V please suggest solution for this rest of the data links seems to be fine.

i have attached a image of the topology and the waveforms.

ラベル(1)
0 件の賞賛
返信
1 解決策
4,827件の閲覧回数
JerryFan
NXP Employee
NXP Employee

1. Per the topology.jpg, the Rt was pull down to the GND, while I think it should be pull up to DDR_VTT(0.75V) and connected to GND with a capacitor. Please refer i.mx6dq CPU board schematic.

2. I don't know the simulation and ISIB model. But for i.mx6dq DDR pad, the drive strength can be configured.What drive strength you are using? Try other value if you can. 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,828件の閲覧回数
JerryFan
NXP Employee
NXP Employee

1. Per the topology.jpg, the Rt was pull down to the GND, while I think it should be pull up to DDR_VTT(0.75V) and connected to GND with a capacitor. Please refer i.mx6dq CPU board schematic.

2. I don't know the simulation and ISIB model. But for i.mx6dq DDR pad, the drive strength can be configured.What drive strength you are using? Try other value if you can. 

0 件の賞賛
返信