DDR3 Custom Board Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3 Custom Board Configuration

Jump to solution
2,836 Views
sayi
Contributor II

Hello NXP Team,

I am trying to bring up a custom board which is using imx6 solo processor with different DDR3 SDRAM Configuration

I am trying to understand the following settings on SABRE solo board . Could you please explain

          0x21b001c = 0x04008032

          0x21b001c = 0x8033

          0x21b001c = 0x48031:

Thanks,

Says

Labels (1)
0 Kudos
Reply
1 Solution
2,597 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply
7 Replies
2,598 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply
2,597 Views
sayi
Contributor II

Thanks Igor !! One final question before I close this topic.

- From BSP porting document for configuring DDR3 I see free-scale mentioned about changing the *.cfg file in boards/mx6solosabresd/*.cfg file but I also see Plugin.s file in the same folder that has the same DCD table as the cfg file and from make file I see we are using plugin.s object file.

For board mx6solosabresd:

Could you please clarify if we should change the DCD table in *.cfg or plugin.s it looks like plugin.s is the assembly version of the *.cfg file.

Thanks,

Swapna

0 Kudos
Reply
2,597 Views
igorpadykov
NXP Employee
NXP Employee

Hi Swapna

both options are equal, one can use them

on own choice.

Best regards

igor

0 Kudos
Reply
2,597 Views
sayi
Contributor II

Thank you Igor.

I already saw the reference manual but I am a bit confused with mode register setting.

For Ex: 0x21b001c = 0x04008032

The mode register address is 0x0400 and I couldn't figure this address from the DRAM manufacturer data sheet.

Could you please help?

0 Kudos
Reply
2,597 Views
igorpadykov
NXP Employee
NXP Employee

Hi Says

one can find in comments attached file:

// Mode register writes

setmem /32    0x021b001c =    0x04008032    // MMDC0_MDSCR, MR2 write, CS0

~igor

0 Kudos
Reply
2,596 Views
sayi
Contributor II

Thanks. This was helpful.

- Can we use JTAG to initialize memory? Are there any scripts for JTAG and recommendations from freescale to bring up a custom board based on solo.?

I am looking at the uboot code  board configuration files and they are *.cfg files with Device configuration Tables is this the only place to change the needed for custom board.

Appreciate your time!!

0 Kudos
Reply
2,597 Views
igorpadykov
NXP Employee
NXP Employee

Hi Says

these records performs programming DDR chips Mode registers,

description can be found in sect.45.12.8 MMDC Core Special Command

Register (MMDCx_MDSCR) i.MX6SDL Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf

and datasheets of used DDR parts.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply