DDR2 on i.MX253

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR2 on i.MX253

1,021 Views
andpas
Contributor II

Hello.
I would use DDR2 RAM with an i.MX253, preferring it over mDDR because of lower costs. The problem is the limit to 4 banks memory,
so basically a single chip cannot give me enough memory.
Is there some way to allocate more DDR2 memory, other than use both
the CS lines of the EMI (max two chips)?
Thanks

Labels (1)
0 Kudos
Reply
1 Reply

892 Views
Frias
Contributor V

Hello Andrea,

You can ground the BA2 on the memory side, thus you would be sparing half of its size, but this enables you to use more memory per CS. For instance, if you use a 2Gbit device, you would be able to access 1Gbit which is more than the 512 of the 4 bank devices...

Besides this option, the only other possibility I see would be to use the second chip select.

Best Regards,

Renato 

0 Kudos
Reply