DDR stress test result write to flash_header.S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR stress test result write to flash_header.S

609 Views
wangzh92429
Contributor II

I follow the option 1 in this file.i.MX6/7 DDR Stress Test Tool V3.00 

my config like this and calibration success.But I don't known if this is right setup.

I known need write calibration parameter write into flash_header.S.Is there any documentation on how to write it?I don't understand how to modify this file.

thanks!

企业微信截图_20190327163255.png

0 Kudos
1 Reply

503 Views
igorpadykov
NXP Employee
NXP Employee

Hi wang

there is no documentation for changing flash_header.S, it is necessary

to check Reference Manual with description of MMDC registers, also may be useful

Freescale i.MX6 DRAM Port Application Guide-DDR3 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos