DDR stress test fail on IMX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR stress test fail on IMX6UL

834件の閲覧回数
abhijeet_pawar
Contributor I

Hello,

i'm using custom board of IMX6UL. While performing DDR stress test on IMX6UL i'm getting an message "Error write DCD failed".

  1. Im using the IMX6UL_MMDC_DDR3_register_programming_aid.inc script for testing board. I have tried by un-ticking verify DCD address but result is same.
  2. Also i verified all addresses are within the valid address ranges as per i.MX 6UltraLite Applications Processor Reference Manual.
  3. I have referred  hardware manual for DDR configuration. Checked all the guidelines are matching with our board as per Hardware Development Guide for the i.MX 6UltraLite Applications Processor.

Can anybody help on this issue?

Thanks,

Abhijeet Pawar.

 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

791件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

This may be hardware issue, you can try to check your hardware first.

0 件の賞賛
返信

791件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

You need to check your DDR design firstly in you schematic. And you need to configure your DDR following the script we supply IMX6UL_MMDC_DDR3_register_programming_aid.

If above steps are OK, then do the DDR stress test to ajust the values.

0 件の賞賛
返信