Thanks igor !!!. This is what i exactly looking for.
I am using the MT41K256M16TW-107AIT:P DDR3-L for our custom board. In the imximage.cfg , the configuration also provided for same part number.
I have seen the DDR script aid, which generate the configuration value, https://community.nxp.com/docs/DOC-329899
But in this script aid excle sheet, Memory Type is given upto DDR3-1600, but -107AIT part has speed 1866. This is not listed in the same excle.
Is it fine, in the same excle sheet memorytype kept as is, i.e DDR3-1600 and change the parameter with specify for the -107 AIT in data sheet like tRCD,tRC,tRAS.
In the imximage.cfg file, i saw the delta between part -125 and -107 is calibration register.( i know this values should come from the stress tool which would be fine ) .
I just want to ask, if you have an experience with MT41K256M16TW-107AIT DDR3 part,except calibration values , if i used all values as is from the cfg file for the custom board. Will it work ?
Thanks for your great Support igor !!!
Thanks& Regards,
Surendra