DDR clock frequency scaling not supported with newer linux kernel (5.15+)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR clock frequency scaling not supported with newer linux kernel (5.15+)

832件の閲覧回数
gfkjfgt
Contributor I

Hi, we have a custom board based on IMX8MM. We were looking at the application note: AN12410 (i.MX8M Mini Power consumption measurement) where it describes the IDLE_DDRC_25MHz mode as a way to save power. However the ddrc nodes has been removed from the imx8mm.dtsi device tree here: https://github.com/nxp-imx/linux-imx/commit/2a6b87ca632bce18e519e7b6ce81c5bda89cad0e .

 

Is it not supported anymore to clock down the memory frequency?

What do you suggest to use instead?

 

Regards

 

 

 

 

0 件の賞賛
返信
1 返信

797件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport
Hi @gfkjfgt 
 
I hope you are doing well.
 

What do you suggest to use instead?

=> Yes, In the latest commit the interconnect and ddrc nodes have been removed as described in the link. To save power one can try to use the CCM Clock Gating Register (CCGR) mentioned in the IMX8MMRM.
Kindly refer to section 5.1.6.3 CCGR Interface for more information.
 
Thanks & Regards,
Sanket Parekh
0 件の賞賛
返信