Hi @pengyong_zhang ,
Thanks for your reply. I understand that the Config Tool can support i.MX95.
I can use the REV 15.1 to run the DDR Test on the MX95 EVK board.
But I found problem when using the latest REV 16.1. I tried to load the configuration that I used in REV 15.1. Also, I tried to create new project in REV 16.1. Neither one can work.
I attached the error screenshot.
By the way, I want to know if NXP is going to add the support of i.MX95 to the DDR Tool.
Thanks for your help.