DDR Test Tool fails to write DCD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DDR Test Tool fails to write DCD

跳至解决方案
2,138 次查看
georgemakarov
Contributor III

Hello!
I try to make DDR calibration and stress test.
I use the latest vesrion of NXP DDR Test Tool 3.00 and the latest DDR register programming aid 1.1
My configuration is i.MX6ULL (MCIMX6Y2CVM05AB) and single chip of DDR3 K4B1G1646I-BMMA0CV
When i try to download utility via SDP i got an error "ERROR: Write dcd failed"
I found that following lines in script lead to this error:

 

setmem /32	0x021B001C =	0x02208032	// MMDC0_MDSCR, MR2 write, CS0					
setmem /32	0x021B001C =	0x00008033	// MMDC0_MDSCR, MR3 write, CS0					
setmem /32	0x021B001C =	0x00048031	// MMDC0_MDSCR, MR1 write, CS0					
setmem /32	0x021B001C =	0x15208030	// MMDC0_MDSCR, MR0 write, CS0					
setmem /32	0x021B001C =	0x04008040	// MMDC0_MDSCR, ZQ calibration command sent to device on CS0					

 


I found several topic in community about similar problem, but in this case these registers is allowable.

georgemakarov_0-1642505810459.png

 

PS.
I have another board that was developed 3 years ago with the same MCU and DDR3 chip, and this board accepts this configuration file well without errors. though fails at calibration anyway 


Best regards, George Makarov
标记 (1)
0 项奖励
回复
1 解答
2,097 次查看
georgemakarov
Contributor III

There was some problems in hardware. I've tried to run this test on another custom board, and it passed succesfully

Best regards, George Makarov

在原帖中查看解决方案

2 回复数
2,098 次查看
georgemakarov
Contributor III

There was some problems in hardware. I've tried to run this test on another custom board, and it passed succesfully

Best regards, George Makarov
2,118 次查看
Yuri
NXP Employee
NXP Employee

@georgemakarov 
Hello,

   is it possible to look at the scheme? You may provide it as reply
on my mail.

Regards,
Yuri.

0 项奖励
回复