DDR Stress tester issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Stress tester issue

1,313 Views
wangvictor
Contributor III

Hi All:

I'm going to tune 4G for my customize product.

I'm using i.MX6Q for my cpu.

I'm using DDR_Stress_Tester_V1.0.3 tool to tuning my 4G.

But I can't running the test successfully even I tried many of different value.

Here is what I set the value.

DDR.png

And before I start to test the stress I had set all the settings like below.

未命名.png

After all these settings than I run the stress test.

It will show fail for me.

123.png

How can I solve this problem?

Thanks in Advanced!

Labels (5)
4 Replies

860 Views
jan_spurek
NXP Employee
NXP Employee

Hello Victor,

according to the datasheet for the part that you are using (MT41K512M16) it has 10 column addresses [9:0]. You have set 9 column addresses in your Script Aid. Please, set the correct value and try running the test again.

Best Regards,

Jan

860 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wang

as error text states: pattern should match address so

there is excessive 0xc0000000 bits. This may be hardware layout

error, one can attach jatg debugger and write to address 0x10000000 data

0x10000000, then read back, inspecting waveforms with oscilloscope.

Just for test one can also decrease testing frequency. Check trace lengths

for these bits: they should be less clock length, refer to layout rules given in

i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

860 Views
leihe
Contributor I

hello!

         I have a problem,software tell me chip id is " i.MX6 Solo/DualLite (0x61)" ,when chose "MX6DL" in target item.my chip logo is "MC IMX6S6AVM08AC"  so it need chose "MX6SL" ,is that right? ,but when i chose "MX6SL" DDR_Tester software show me "ERROR: Can't open USB device!!!",can you help me,thankyou! 

         The version of DDR_Tester.exe is  v2.8. i get it in https://community.nxp.com/servlet/JiveServlet/download/105652-38-421997/ddr_stress_tester_v2.80.exe.... 

0 Kudos

860 Views
leihe
Contributor I

MC IMX6S6AVM08AC should chose "MX6DL"

0 Kudos