DDR Stress Tools v2.52 didn't pass low frequency during stress test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Stress Tools v2.52 didn't pass low frequency during stress test

Jump to solution
666 Views
wallyyeh
Contributor V

Hi, All:

   Our new product have some memory issue which old product didn't, we did the calibration test and update the MMDC registers(uboot/board/freescale/mx6q_sabresd/flash_header.S). now it can pass DDR stress test for range 413 ~ 585MHz. (but old product can pass 413~672MHz)

   According Freescale i.MX6 DRAM Port Application Guide-DDR3 , in page 19, it says:

If the DDR3 cannot even pass the stress test at a low frequency, say 200 MHz, it is more likely to be a

hardware problem. Then, it would be a good starting point to check the DDR3 connections. In addition,

you should check the power supply for the DDR3, i.MX6 MMDC and DDR3 I/O to see if voltage is valid

and ripple is not too large.

    Our new product never success on frequency lower than 400Mhz, is this situation just fine or not?

Labels (1)
Tags (1)
0 Kudos
1 Solution
503 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wally

yes it should pass lower frequency DDR stress test

Best regards

igor

View solution in original post

0 Kudos
3 Replies
503 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wally

one can check with oscilloscope power supplies ripples (should be <5%) and

ddr signals waveforms . Also one can experiment to determine if it is a

hardware PCB issue: hand solder 22uF capacitors directly under center of chip.

May be recommended to tweak with drive strength settings.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

503 Views
wallyyeh
Contributor V

Dear igorpadykov:

    Thanks for reply. :smileyhappy:

so our product "should" pass the lower frequency DDR stress test, right?

I'll tell HW partner to check the advice which you give.

0 Kudos
504 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wally

yes it should pass lower frequency DDR stress test

Best regards

igor

0 Kudos