DDR_Stress_Tester for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR_Stress_Tester for i.MX6

Jump to solution
1,584 Views
norton
Contributor II

Does the USB driver that comes with the ddr_stress_tester support the i.MX6?

Labels (1)
1 Solution
951 Views
TheAdmiral
NXP Employee
NXP Employee

Hi Michael,

The technical answer to your question is: No. The USB driver that comes with the ddr_stress_tester does not support i.MX6.

The reason is that the i.MX6 is USB coded as a Human Interface Device (HID), and therefore, does not need special USB drivers.

The USB drivers are for i.MX53 and earlier processors. i.MX6 does not need a special driver.

Cheers,

Mark

View solution in original post

2 Replies
951 Views
YixingKong
Senior Contributor IV

Michael, please click Correct Answer/Helpful Anwer, if your question has been answered.

Thanks,

Yixing

0 Kudos
Reply
952 Views
TheAdmiral
NXP Employee
NXP Employee

Hi Michael,

The technical answer to your question is: No. The USB driver that comes with the ddr_stress_tester does not support i.MX6.

The reason is that the i.MX6 is USB coded as a Human Interface Device (HID), and therefore, does not need special USB drivers.

The USB drivers are for i.MX53 and earlier processors. i.MX6 does not need a special driver.

Cheers,

Mark