I can start the android system and also use the console, but I can't use the DDR_Stress_Tester_for MX51_MX53 tools.
The error info :
rom_check_hab: reading ERROR ack failed 0x0
rom_check_hab<> failed
I have encountered before, but the solution.
You must determine the UART1 .boot0 and boot1 are 1.8V
the Serial toolsVCC is 3.3V
I've put the CPU in Serial mode and Run DDR test, It's giving below output.
--------------------------------------------------------------------------
HAB_TYPE: DEVELOP
Image loading...
download Image to IRAM OK
Running DDR test..., press "ESC" key to exit.
rom_exec: reading ERROR ack failed 0x00000000
--------------------------------------------------------------------------
Does above output means DDR test is failed? OR Is it still running?
Is there source code available for this stress tester tool(DDR_Stress_Tester_for MX51_MX53)?
i.MX53 should be in serial (UART / USB) boot mode for the DDR stress tester.