DDR_Stress_Tester_for MX51_MX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR_Stress_Tester_for MX51_MX53

1,474 Views
Danial
Contributor II

I can start the android system and also use the console,  but I can't use the DDR_Stress_Tester_for MX51_MX53 tools.

The error info :

rom_check_hab: reading ERROR ack failed 0x0

rom_check_hab<> failed

0 Kudos
4 Replies

804 Views
zhangyinhua
Contributor I

I have encountered before, but the solution.

You must determine the UART1 .boot0 and boot1 are 1.8V

the Serial toolsVCC is 3.3V

0 Kudos

804 Views
Danial
Contributor II
I had set cpu in serial mod, I can use the tools on the QSB board. Thanks!
0 Kudos

804 Views
vishnupatekar
Contributor II

I've put the CPU in Serial mode and Run DDR test, It's giving below output.

--------------------------------------------------------------------------

HAB_TYPE: DEVELOP

Image loading...

download Image to IRAM OK

Running DDR test..., press "ESC" key to exit.

rom_exec: reading ERROR ack failed 0x00000000

--------------------------------------------------------------------------

Does above output means DDR test is failed? OR Is it still running?

Is there source code available for this stress tester tool(DDR_Stress_Tester_for MX51_MX53)?

0 Kudos

804 Views
Yuri
NXP Employee
NXP Employee

i.MX53 should be in serial (UART / USB) boot mode for the DDR stress tester.

0 Kudos