DDR_Stress_Tester_for MX51_MX53 程序可以正常运行,但是log代表什么意思?

cancel
Showing results for 
Search instead for 
Did you mean: 

DDR_Stress_Tester_for MX51_MX53 程序可以正常运行,但是log代表什么意思?

483 Views
cloudxxcloud
Contributor I

t4: IRAM_to_DDRv2 test
t5: IRAM_to_DDRv1 test
t6: read noise walking ones and zeros test

2298
t0: memcpy11 SSN test
t1: memcpy8 SSN test
t2: memcpy11 random pattern test
t3: byte-wise SSN test
t4: IRAM_to_DDRv2 test
t5: IRAM_to_DDRv1 test
t6: read noise walking ones and zeros test

2299
t0: memcpy11 SSN test
t1: memcpy8 SSN test
t2: memcpy11 random pattern test
t3: byte-wise SSN test
t4: IRAM_to_DDRv2 test
t5: IRAM_to_DDRv1 test
t6: read noise walking ones and zeros test

2300
t0: memcpy11 SSN test
t1: memcpy8 SSN test

 

2200,2300这些数代表什么意思?

什么时候这个程序可以停下来?

 

 

0 Kudos
3 Replies

460 Views
BiyongSUN
NXP Employee
NXP Employee

这些数字是测试次数。 

做一次  标准的 t0 到  t6  压力测试 加1

不停下来时这样可以做 over night 测试 

0 Kudos

463 Views
b45499
NXP TechSupport
NXP TechSupport

没出错的话,可以不管的

0 Kudos

479 Views
cloudxxcloud
Contributor I

微信图片_20220318174403.png

0 Kudos