Hello,
Software/ Hardware details,
L4.14.98 + IMX8QM Custom Board
SCFW 1.2.1
RPA: V17
ER8
I got the following response from DDR Stress Test,
If you want to watch DDR script executing process, please open SCU debug uart in other serial tool
Waiting for the target board boot...
Hi Vinothkumar
reason for that behaviour may wrongly configured uart, one can look at below link "FAQs:"
Also recommended to attach another terminal to " SCU debug uart" as suggests ddr test log.
Best regards
igor
Thank you @igorpadykov for the reply.
Also recommended to attach another terminal to " SCU debug uart" as suggests ddr test log.
<Vinoth> Currently there is one debug UART in custom board. Is it enough to do the DDR Stress Test ?
Hi @igorpadykov
My custom board hanged here, I unable to find out the any log due to one debug uart in custom board by default.
i.MX8QM_B0 is found
Download is complete£¡
If you want to watch DDR script executing proces, please open SCU debug uart in other serial tool
Waiting for the target board boot...
I got the following log from DDR Stress Test Tool. But, the hardware is limited to one debug uart (UART1).
Is it possible to enable/route all message through one debug UART ?.
Will you please provide the SCFW board configuration file (with modified debug uart) for UART1 for SCU UART.
or Do I needs to do any hardware modification ?