I have a problem very similar to DDR stress tester v1.0.2 with i.MX6DL error , except it works on other computers reliably, but fails to run on my computer. In the past it has run on my computer, but I don't know what has changed. The following is the only text that is displayed before going to the command prompt.
C:\DDR_Stress_Tester_V1.0.3\Binary>DDR_Stress_Tester.exe -t mx6x -df scripts\MX6_series_boards\SabreSD\RevC_and_RevB\MX6DL\MX6DL_SabreSD_DDR3_register_programming_aid_v1.5.inc
MX6DL opened.
HAB_TYPE: DEVELOP
rom_write: reading CMD ack failed 0x00000000
ROM Write failed, addr: 0x020e0764
Write dcd failed.
I have tried plugging it into other USB ports hoping it was an initialization problem, and I have tried other boards. Does anyone have any ideas?
Solved! Go to Solution.
As for "ERROR: Write dcd failed" - please takea look at
DDR stress tester V2.00 problem with i.MX6 solo lite interfacing with DDR3
Regards,
Yuri.
Hello,
Please try the i.MX6/7 DDR Stress Test Tool V2.10
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I like the new stress tester, however it is also not working for me. I am getting the following message:
ERROR: Write dcd failed.
Which is essentially the same thing the v1.03 tester was giving me.
I've tried restarting the computer, redownloading the v1.03 as well as the v2.10, none of which has worked. The thing that really bothers me is that everything is still working on other computers.
As for "ERROR: Write dcd failed" - please takea look at
DDR stress tester V2.00 problem with i.MX6 solo lite interfacing with DDR3
Regards,
Yuri.