DDR Stress Test failed for IMX8DX Custom Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Stress Test failed for IMX8DX Custom Board

2,193 Views
songhongliang
Contributor II

 

hi  nxp

my board cpu is imd8dx 16bit LPDDR4,please the fail, Can you provide me with some help to fix the error。


*************************************************************************
MX8 DDR Stress Test Version: ER14
Built on Mar 27 2020 12:28:23
*************************************************************************

--Set up the MMU and enable I and D cache--
- This is the Cortex-A35 core
- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTBR0_EL3
- Config TCR_EL3
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug

- VMCR Check:
- ttbr0_el3: 0x13d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x101122

- MMU and cache setup complete

*************************************************************************
ARM Clock(CA35): 1200MHz
DDR Clock: 1200MHz

============================================
DDR configuration
DDR type is LPDDR4
Data width: 16, bank num: 8
Row size: 16, col size: 10
One chip select is used
Number of DDR controllers used on the SoC: 1
Density per chip select: 1024MB
Density per controller is: 1024MB
Total density detected on the board is: 1024MB

 

********************************************
WARNING! DDR training errors were detected on DDRC 0!
DDR_PHY_PGSR0 = 0x806cc07f
DQS Gate training error detected
Write Leveling training error detected
VREF training error detected
Write DQS2DQ training error detected
Recheck DDR initialization
********************************************
============================================

MX8QXP: Cortex-A35 is found

0 Kudos
Reply
3 Replies

2,189 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hongliang

 

since all trainings are with errors, one can check with oscilloscope if there are any signals

on memory. Also recommended to use latest MX8DualX_C0_B0_LPDDR4_RPA_1.2GHz_v16.xlsx on

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QXP-DXP-DX-DDR-Register-Programming...

 

Best regards
igor

0 Kudos
Reply

2,184 Views
songhongliang
Contributor II

HI,

I have used the latest scfw1.7.0 and MX8DualX_C0_B0_LPDDR4_RPA_1.2GHz_v16.xls。

 

0 Kudos
Reply

2,181 Views
igorpadykov
NXP Employee
NXP Employee

>I have used the latest scfw1.7.0..

 

it is not latest, latest is v1.10.0  SCFW Porting Kit​ 1.10.0

 

Best regards
igor

0 Kudos
Reply