DDR Calibration on iMx6 DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Calibration on iMx6 DL

1,150 Views
dhanunjay
Contributor III

Hi ALL,

I have changed some of the drive strength parameters in DDR config code, all DDR calibration tests are passing.

But I configured Write levelling parameters as:

     0x021b080c =     0x001F001F   

     0x021b0810 =     0x001F001F   

     0x021b480c =     0x001F001F   

     0x021b4810 =     0x001F001F

and output values are:

Start write leveling calibration

Write leveling calibration completed

Start write leveling calibration

Write leveling calibration completed

MMDC_MPWLDECTRL0 ch0 after write level cal: 0x004E0051

MMDC_MPWLDECTRL1 ch0 after write level cal: 0x00420048

MMDC_MPWLDECTRL0 ch1 after write level cal: 0x00330031

MMDC_MPWLDECTRL1 ch1 after write level cal: 0x0030003F

could please help me, the output values are larger than configured values?

Do i need to change any configuration parameters.

Please suggest me.

Labels (1)
0 Kudos
3 Replies

729 Views
dhanunjay
Contributor III

Dear NxP support Team,

Issue: After executing DDR calibration code, not able to load application from flash memory.

We have integrated DDR calibration source code(provided by nxp, version 1.0.2) to our customized boot loader. After clock, pinmux, and ddr initilization, we executed the DDR calibration tests(writeleveling, DQS gating, read & write calibration). After executing DDR calibration tests, not running the system.

it some times hangs in uart initilization...etc.

results:

Start write leveling calibration

Write leveling calibration completed

MMDC_MPWLDECTRL0 ch0 after write level cal: 0x00500058

MMDC_MPWLDECTRL1 ch0 after write level cal: 0x0042004B

MMDC_MPWLDECTRL0 ch1 after write level cal: 0x00330035

MMDC_MPWLDECTRL1 ch1 after write level cal: 0x0036004B

Starting DQS gating calibration...

. HC_DEL=0x       0     result[ 0]=0x 1001011

. HC_DEL=0x       1     result[ 1]=0x    1001

. HC_DEL=0x       2     result[ 2]=0x       0

. HC_DEL=0x       3     result[ 3]=0x11000000

. HC_DEL=0x       4     result[ 4]=0x11111111

. HC_DEL=0x       5     result[ 5]=0x11111111

. HC_DEL=0x       6     result[ 6]=0x11111111

. HC_DEL=0x       7     result[ 7]=0x11111111

. HC_DEL=0x       8     result[ 8]=0x11111111

. HC_DEL=0x       9     result[ 9]=0x11111111

. HC_DEL=0x       A     result[ A]=0x11111111

. HC_DEL=0x       B     result[ B]=0x11111111

. HC_DEL=0x       C     result[ C]=0x11111111

. HC_DEL=0x       D     result[ D]=0x11111111

DQS HC delay value low1 = 0x     406, high1=0x 605070C

DQS HC delay value low2 = 0x 5090202, high2=0x B0B0505

loop ABS offset to get HW_DG_LOW

. ABS_OFFSET=0x       0 result[ 0]=0x11001001

. ABS_OFFSET=0x       4 result[ 1]=0x11001001

. ABS_OFFSET=0x       8 result[ 2]=0x11001001

. ABS_OFFSET=0x       C result[ 3]=0x11001001

. ABS_OFFSET=0x      10 result[ 4]=0x11001001

. ABS_OFFSET=0x      14 result[ 5]=0x11001001

. ABS_OFFSET=0x      18 result[ 6]=0x11001001

. ABS_OFFSET=0x      1C result[ 7]=0x11001001

. ABS_OFFSET=0x      20 result[ 8]=0x11001001

. ABS_OFFSET=0x      24 result[ 9]=0x11001011

. ABS_OFFSET=0x      28 result[ A]=0x11001011

. ABS_OFFSET=0x      2C result[ B]=0x11001011

. ABS_OFFSET=0x      30 result[ C]=0x11001011

. ABS_OFFSET=0x      34 result[ D]=0x11001011

. ABS_OFFSET=0x      38 result[ E]=0x11001011

. ABS_OFFSET=0x      3C result[ F]=0x11001011

. ABS_OFFSET=0x      40 result[10]=0x11001011

. ABS_OFFSET=0x      44 result[11]=0x11001011

. ABS_OFFSET=0x      48 result[12]=0x11001011

. ABS_OFFSET=0x      4C result[13]=0x11001011

. ABS_OFFSET=0x      50 result[14]=0x11001011

. ABS_OFFSET=0x      54 result[15]=0x11001011

. ABS_OFFSET=0x      58 result[16]=0x11001011

. ABS_OFFSET=0x      5C result[17]=0x11001011

. ABS_OFFSET=0x      60 result[18]=0x11001011

. ABS_OFFSET=0x      64 result[19]=0x11001011

. ABS_OFFSET=0x      68 result[1A]=0x11001011

. ABS_OFFSET=0x      6C result[1B]=0x11001011

. ABS_OFFSET=0x      70 result[1C]=0x11001011

. ABS_OFFSET=0x      74 result[1D]=0x11001011

. ABS_OFFSET=0x      78 result[1E]=0x11001011

. ABS_OFFSET=0x      7C result[1F]=0x11001011

loop ABS offset to get HW_DG_HIGH

. ABS_OFFSET=0x       0 result[ 0]=0x11111111

. ABS_OFFSET=0x       4 result[ 1]=0x11111111

. ABS_OFFSET=0x       8 result[ 2]=0x11111111

. ABS_OFFSET=0x       C result[ 3]=0x11111111

. ABS_OFFSET=0x      10 result[ 4]=0x11111111

. ABS_OFFSET=0x      14 result[ 5]=0x11111111

. ABS_OFFSET=0x      18 result[ 6]=0x11111111

. ABS_OFFSET=0x      1C result[ 7]=0x11111111

. ABS_OFFSET=0x      20 result[ 8]=0x11111111

. ABS_OFFSET=0x      24 result[ 9]=0x11111111

. ABS_OFFSET=0x      28 result[ A]=0x11111111

. ABS_OFFSET=0x      2C result[ B]=0x11111111

. ABS_OFFSET=0x      30 result[ C]=0x11111111

. ABS_OFFSET=0x      34 result[ D]=0x11111111

. ABS_OFFSET=0x      38 result[ E]=0x11111111

. ABS_OFFSET=0x      3C result[ F]=0x11111111

. ABS_OFFSET=0x      40 result[10]=0x11111111

. ABS_OFFSET=0x      44 result[11]=0x11111111

. ABS_OFFSET=0x      48 result[12]=0x11111111

. ABS_OFFSET=0x      4C result[13]=0x11111111

. ABS_OFFSET=0x      50 result[14]=0x11111111

. ABS_OFFSET=0x      54 result[15]=0x11111111

. ABS_OFFSET=0x      58 result[16]=0x11111111

. ABS_OFFSET=0x      5C result[17]=0x11111111

. ABS_OFFSET=0x      60 result[18]=0x11111111

. ABS_OFFSET=0x      64 result[19]=0x11111111

. ABS_OFFSET=0x      68 result[1A]=0x11111111

. ABS_OFFSET=0x      6C result[1B]=0x11111111

. ABS_OFFSET=0x      70 result[1C]=0x11111111

. ABS_OFFSET=0x      74 result[1D]=0x11111111

. ABS_OFFSET=0x      78 result[1E]=0x11111111

. ABS_OFFSET=0x      7C result[1F]=0x11111111

BYTE 0:

        Start:           HC=0x 5 ABS=0x 0

        End:             HC=0x C ABS=0x20

        Mean:            HC=0x 8 ABS=0x4F

        End-0.5*tCK:     HC=0x B ABS=0x20

        Final:           HC=0x B ABS=0x20

BYTE 1:

        Start:           HC=0x 3 ABS=0x 0

        End:             HC=0x 7 ABS=0x20

        Mean:            HC=0x 5 ABS=0x10

        End-0.5*tCK:     HC=0x 6 ABS=0x20

        Final:           HC=0x 6 ABS=0x20

BYTE 2:

        Start:           HC=0x 0 ABS=0x 0

        End:             HC=0x 5 ABS=0x78

        Mean:            HC=0x 2 ABS=0x7B

        End-0.5*tCK:     HC=0x 4 ABS=0x78

        Final:           HC=0x 4 ABS=0x78

BYTE 3:

        Start:           HC=0x 0 ABS=0x 0

        End:             HC=0x 6 ABS=0x78

        Mean:            HC=0x 3 ABS=0x3C

        End-0.5*tCK:     HC=0x 5 ABS=0x78

        Final:           HC=0x 5 ABS=0x78

BYTE 4:

        Start:           HC=0x 1 ABS=0x 0

        End:             HC=0x 5 ABS=0x C

        Mean:            HC=0x 3 ABS=0x 6

        End-0.5*tCK:     HC=0x 4 ABS=0x C

        Final:           HC=0x 4 ABS=0x C

BYTE 5:

        Start:           HC=0x 1 ABS=0x 8

        End:             HC=0x 5 ABS=0x C

        Mean:            HC=0x 3 ABS=0x A

        End-0.5*tCK:     HC=0x 4 ABS=0x C

        Final:           HC=0x 4 ABS=0x C

BYTE 6:

        Start:           HC=0x 8 ABS=0x 0

        End:             HC=0x B ABS=0x70

        Mean:            HC=0x 9 ABS=0x77

        End-0.5*tCK:     HC=0x A ABS=0x70

        Final:           HC=0x A ABS=0x70

BYTE 7:

        Start:           HC=0x 4 ABS=0x 0

        End:             HC=0x B ABS=0x78

        Mean:            HC=0x 7 ABS=0x7B

        End-0.5*tCK:     HC=0x A ABS=0x78

        Final:           HC=0x A ABS=0x78

DQS calibration MMDC0 MPDGCTRL0 = 0x46200B20, MPDGCTRL1 = 0x 5780478

DQS calibration MMDC1 MPDGCTRL0 = 0x440C040C, MPDGCTRL1 = 0x A780A70

Note: Array result[] holds the DRAM test result of each byte.

      0: test pass.  1: test fail

      4 bits respresent the result of 1 byte.

      result 00000001:byte 0 fail.

      result 00000011:byte 0, 1 fail.

Starting Read calibration...

ABS_OFFSET=0x       0   result[ 0]=0x11111111

ABS_OFFSET=0x 4040404   result[ 1]=0x11111111

ABS_OFFSET=0x 8080808   result[ 2]=0x11111111

ABS_OFFSET=0x C0C0C0C   result[ 3]=0x11111111

ABS_OFFSET=0x10101010   result[ 4]=0x11111111

ABS_OFFSET=0x14141414   result[ 5]=0x11111111

ABS_OFFSET=0x18181818   result[ 6]=0x11111111

ABS_OFFSET=0x1C1C1C1C   result[ 7]=0x11111111

ABS_OFFSET=0x20202020   result[ 8]=0x11111111

ABS_OFFSET=0x24242424   result[ 9]=0x11111111

ABS_OFFSET=0x28282828   result[ A]=0x11111111

ABS_OFFSET=0x2C2C2C2C   result[ B]=0x11111111

ABS_OFFSET=0x30303030   result[ C]=0x11111111

ABS_OFFSET=0x34343434   result[ D]=0x 1111111

ABS_OFFSET=0x38383838   result[ E]=0x 1111111

ABS_OFFSET=0x3C3C3C3C   result[ F]=0x 1111111

ABS_OFFSET=0x40404040   result[10]=0x11111111

ABS_OFFSET=0x44444444   result[11]=0x11111111

ABS_OFFSET=0x48484848   result[12]=0x11111111

ABS_OFFSET=0x4C4C4C4C   result[13]=0x11111111

ABS_OFFSET=0x50505050   result[14]=0x11111111

ABS_OFFSET=0x54545454   result[15]=0x11111111

ABS_OFFSET=0x58585858   result[16]=0x11111111

ABS_OFFSET=0x5C5C5C5C   result[17]=0x11111111

ABS_OFFSET=0x60606060   result[18]=0x11111111

ABS_OFFSET=0x64646464   result[19]=0x11111111

ABS_OFFSET=0x68686868   result[1A]=0x11111111

ABS_OFFSET=0x6C6C6C6C   result[1B]=0x11111111

ABS_OFFSET=0x70707070   result[1C]=0x11111111

ABS_OFFSET=0x74747474   result[1D]=0x11111111

ABS_OFFSET=0x78787878   result[1E]=0x11111111

ABS_OFFSET=0x7C7C7C7C   result[1F]=0x11111111

MMDC0 MPRDDLCTL = 0x70006E6E, MMDC1 MPRDDLCTL = 0x30347272

Starting Write calibration...

ABS_OFFSET=0x       0   result[ 0]=0x11111111

ABS_OFFSET=0x 4040404   result[ 1]=0x11111111

ABS_OFFSET=0x 8080808   result[ 2]=0x11111111

ABS_OFFSET=0x C0C0C0C   result[ 3]=0x11111111

ABS_OFFSET=0x10101010   result[ 4]=0x11111111

ABS_OFFSET=0x14141414   result[ 5]=0x11111111

ABS_OFFSET=0x18181818   result[ 6]=0x11111111

ABS_OFFSET=0x1C1C1C1C   result[ 7]=0x 1111111

ABS_OFFSET=0x20202020   result[ 8]=0x 1111111

ABS_OFFSET=0x24242424   result[ 9]=0x11111111

ABS_OFFSET=0x28282828   result[ A]=0x11111111

ABS_OFFSET=0x2C2C2C2C   result[ B]=0x11111111

ABS_OFFSET=0x30303030   result[ C]=0x11111111

ABS_OFFSET=0x34343434   result[ D]=0x11111111

ABS_OFFSET=0x38383838   result[ E]=0x11111111

ABS_OFFSET=0x3C3C3C3C   result[ F]=0x11111111

ABS_OFFSET=0x40404040   result[10]=0x11111111

ABS_OFFSET=0x44444444   result[11]=0x11111111

ABS_OFFSET=0x48484848   result[12]=0x11111111

ABS_OFFSET=0x4C4C4C4C   result[13]=0x11111111

ABS_OFFSET=0x50505050   result[14]=0x11111111

ABS_OFFSET=0x54545454   result[15]=0x11111111

ABS_OFFSET=0x58585858   result[16]=0x11111111

ABS_OFFSET=0x5C5C5C5C   result[17]=0x11111111

ABS_OFFSET=0x60606060   result[18]=0x11111111

ABS_OFFSET=0x64646464   result[19]=0x11111111

ABS_OFFSET=0x68686868   result[1A]=0x11111111

ABS_OFFSET=0x6C6C6C6C   result[1B]=0x11111111

ABS_OFFSET=0x70707070   result[1C]=0x11111111

ABS_OFFSET=0x74747474   result[1D]=0x11111111

ABS_OFFSET=0x78787878   result[1E]=0x11111111

ABS_OFFSET=0x7C7C7C7C   result[1F]=0x11111111

MMDC0 MPWRDLCTL = 0x70683838,MMDC1 MPWRDLCTL = 0x24206E6E

   MMDC registers updated from calibration

   Read DQS Gating calibration

   MPDGCTRL0 PHY0 (0x021b083c) = 0x46200B20

   MPDGCTRL1 PHY0 (0x021b0840) = 0x05780478

   MPDGCTRL0 PHY1 (0x021b483c) = 0x440C040C

   MPDGCTRL1 PHY1 (0x021b4840) = 0x0A780A70

   Read calibration

   MPRDDLCTL PHY0 (0x021b0848) = 0x70006E6E

   MPRDDLCTL PHY1 (0x021b4848) = 0x30347272

   Write calibration

   MPWRDLCTL PHY0 (0x021b0850) = 0x70683838

   MPWRDLCTL PHY1 (0x021b4850) = 0x24206E6E

0 Kudos

729 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please try the recent DDR Stress test :

https://community.nxp.com/docs/DOC-105652 

Regards,

Yuri.

0 Kudos

729 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I do not think that it is required to change calibration values, if memory

tests are passed after initialization with found calibration values.

Nevertheless, please take a look at section 3.1.1 (Write Leveling Calibration)

of Freescale i.MX6 DRAM Port Application Guide-DDR3


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos