DDR Calibration on i.MX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Calibration on i.MX53

Jump to solution
3,551 Views
KarelH
Contributor II

Hello,

could anybody please explain how to make DDR calibration or how to obtain calibration values?

I know there is DDR Stress Tester, but it gives no useful results.

I know there is the document AN4466 i.MX53 DDR Calibration and there are some example codes, but I don't know how to use it.

Do I need to make a program which I load to IRAM?

Thank you,

Karel

Labels (1)
0 Kudos
Reply
1 Solution
2,864 Views
igorpadykov
NXP Employee
NXP Employee

Hi Karel

please look at attached example.

Yes, you need to make a program which loads to IRAM.

Actually i.MX53 DDR calibration is rarely used, just because with

good DDR routing it is not necessary at all. It can just compensate small

timing shiftings, but not compensate overall bad DDR routing.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
9 Replies
2,864 Views
pawelkrzyzanows
Contributor II

I just manage to do same things with i.mx6 so will post answer to Your question.

If You need DDR callibration You can use freescale tool: DDR stress tester as You said. In outputs there are results with few registers e.g. MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x0036002D

Later when You build custom U-Boot (or Image) those values needed to be set. If You use embest u-boot: git://github.com/embest-tech/u-boot-imx.git -b embest_imx_3.0.35_4.0.0   in   board/freescale/..../flash_header.s   You have to put values from tool.


After You have Your u-boot prepared You can put it to board with official MFG_tool. Or If you work on Linux You can use imx_usb tool (not supported on this forum :smileygrin:)

0 Kudos
Reply
2,864 Views
osmarfrisonjun1
Contributor III

DDR Stress for MX53 don't have outputs.

It is the reason to use the example (calibration.c) posted here.

So, the question is: How to use it?

0 Kudos
Reply
2,864 Views
igorpadykov
NXP Employee
NXP Employee

SDRAM calibration procedures are described in the

following app note AN4466 :    i.MX53 DDR Calibration. 

http://cache.freescale.com/files/32bit/doc/app_note/AN4466.pdf

~igor

0 Kudos
Reply
2,864 Views
osmarfrisonjun1
Contributor III

0 Kudos
Reply
2,864 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply
2,864 Views
osmarfrisonjun1
Contributor III

Hello

I followed the steps at the Integrating Processor Expert for i.MX and ARM GCC with Eclipse and I built a helloworld program.

I tested it at the user space and it run perfectly.

When I load it to iRAM, "data abort" appears and the board reboots automatically.

/* Log */

=> fatload mmc 0:1 0xF8000000 helloworld

reading helloworld

10174 bytes read in 17 ms (584 KiB/s)

=> go 0xF8000000

## Starting application at 0xF8000000 ...

data abort

pc : [<f8000028>]          lr : [<8ff63fe8>]

reloc pc : [<df8a1028>]    lr : [<77804fe8>]

sp : 8f55cd68  ip : 00000030     fp : 8f6dabc8

r10: 00000002  r9 : 8f55cec8     r8 : 00000000

r7 : 8f5622b0  r6 : f8000000     r5 : 00000002  r4 : 8f5622b4

r3 : f8000000  r2 : 8f5622b4     r1 : 8f5622b4  r0 : 00000000

Flags: nZCv  IRQs off  FIQs off  Mode SVC_32

Resetting CPU ...

resetting ...

U-Boot 2015.04+fslc+g5d9ffd2 (Nov 11 2015 - 10:00:24)

Board: MX53 LOCO

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1

In:    serial

Out:   serial

Err:   serial

Net:   FEC

Error: FEC address not set.

.......

0 Kudos
Reply
2,865 Views
igorpadykov
NXP Employee
NXP Employee

Hi Karel

please look at attached example.

Yes, you need to make a program which loads to IRAM.

Actually i.MX53 DDR calibration is rarely used, just because with

good DDR routing it is not necessary at all. It can just compensate small

timing shiftings, but not compensate overall bad DDR routing.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,864 Views
osmarfrisonjun1
Contributor III

Hello

Can you explain how to use this example? (compilation, load to iram, execution...)

I don't have JTAG interface in my custom board.

Thanks.

0 Kudos
Reply
2,864 Views
KarelH
Contributor II

Thank you for reply and the code. So I hope the calibration will not be necessary.

I'm currently using Linux and LTIB, so I don't know how to compile small program like this. Could you please point me to some info?

Or is there any compiled utility for calibration for i.MX53?

0 Kudos
Reply