DCSS issue on imx8m quadlite with 4.14.78

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DCSS issue on imx8m quadlite with 4.14.78

612 Views
jared_kung
Contributor I

We encountered "dcss is diabled on i.MX8MQL" with L4.14.78 kernel on our board. The processor is iMX8M QuadLite.

So we can't use HDMI. But no this issue with L4.9.88 kernel.

=====================================================

U-Boot 2018.03_xxxx (May 06 2019 - 10:11:22 +0800)

CPU: Freescale i.MX8MQLite rev2.0 1300 MHz (running at 800 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 0C
Reset cause: POR
Model: xxxxx xxx iMX8M
DRAM: 2 GiB
tcpc_init: Can't find device id=0x50
setup_typec: tcpc init failed, err=-19
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... OK
No panel detected: default to HDMI
dcss is diabled on i.MX8MQL
LCD HDMI cannot be configured: -1
In: serial
Out: serial
Err: serial

BuildInfo:
- ATF dc54edb
- U-Boot 2018.03_xxxxxx

======================================================

BR,

Jared

Labels (1)
0 Kudos
1 Reply

460 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jared

one can try latest L4.14.98 as it has additional DCSS fuse check :

check_dcss_fused()

soc.c\imx8m\mach-imx\arm\arch - uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos