DATAIO image creation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DATAIO image creation

2,593 Views
jacklu
Contributor II

Hi,

In IMX6SL platform, is DATAIO image supported? We want to do the EMMC download before factory SMT.

Thanks!

Labels (2)
Tags (1)
0 Kudos
Reply
4 Replies

2,431 Views
igorpadykov
NXP Employee
NXP Employee

Hi jack

yes, one can write image to emmc before soldering it on board,

please refer to sect.4.3 Preparing an SD/MMC card to boot

attached document.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,431 Views
jacklu
Contributor II

Dear Igorpadykov,

I really appreciate your help.

Our project is an android proj, so, this document is a little different from our requirement.

Could you help to release the method for DATAIO on android?

Thank You!

BRs,

Jack

0 Kudos
Reply

2,431 Views
igorpadykov
NXP Employee
NXP Employee

Hi jack

please refer to attached file sect.4.1.3 Downloading images with dd utility

Best regards

igor

2,431 Views
jacklu
Contributor II

Hi Igorpadykov,

Thank you.

I will try it.

BRs,

Jack

0 Kudos
Reply