DART6UL - imx6ull wlan0 not available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DART6UL - imx6ull wlan0 not available

1,212 Views
julenarregi
Contributor I

Hi,

I'm working with the DART-6UL from Variscite, which has the i.MX 6Ultralite processor. I've built Yocto Morty 2.2.1 Linux distribution from Variscite for it and the image is "core-image-minimal". The kernel version is 4.1.15.

When I try to set wlan0 interface up, I get the following error:

   root@imx6ul-var-dart:~# ifconfig wlan0 up

   ifconfig: siocgifflags: no such device

In the device tree everything seems to be added for the wifi to work. And from the OS that came flashed from the manufacturer I know that the hardware is fine and I can connect to wireless networks without problems.

What should I add to my "core-image-minimal" image to get a working WiFi?

Thanks in advance,

Julen

Labels (4)
0 Kudos
1 Reply

811 Views
julenarregi
Contributor I

had to add packagegroups-base and everything is working as expected!

0 Kudos