Customize uboot for imx6Solo (not imxSoloLite) based hardware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Customize uboot for imx6Solo (not imxSoloLite) based hardware

1,443 Views
PraveenM
Contributor I

Hi,

I am working on creating uboot binary for a customized board based on imx6Solo. The Board Boot settings have been hardwired to boot from SD2.

Which one would be the best reference uboot? sabreSd or imxsl_evk ?

Thanks.

Labels (1)
0 Kudos
Reply
3 Replies

1,277 Views
igorpadykov
NXP Employee
NXP Employee

Hi PraveenM

for Solo one needs to use i.MX6DL Sabre SD reference board design.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,277 Views
PraveenM
Contributor I

Hi Igor,

Thanks for the response.

I have downloaded the uboot version 2014.3.10.53_1.1.0_ga. In this, I could see a configuration imx6SoloSabreSd.

I have a question: Where do we configure the size of the DDR. I see the auto-generated config.h file getting the DDR size as 512MB from somewhere.

0 Kudos
Reply

1,277 Views
PraveenM
Contributor I

I answered my question.

I will use the mx6sabresd with mx6solosabresd configuration and customize it for our board.

Thanks for the help.

0 Kudos
Reply