Custom i.mx23 board rom error code 0x80502008 .

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Custom i.mx23 board rom error code 0x80502008 .

3,629 次查看
RandyGraham
Contributor IV

Hello,

We are trying to boot a custom i.mx23 board from an sd card and are seeing the following rom error code.

//! 0x80502008

#define ERROR_ROM_USB_CONNECT_TIMEOUT        (ERROR_ROM_GROUP |

ERROR_ROM_USB_DRIVER_GROUP | 0x8)


It does not appear to attempt to boot from the sd card.


Does the error above prevent it from booting from sd ?


We are looking for hardware issues but I was wondering if anyone had any insights into how this error affects boot, etc.


Thanks for any help,


-Randy


标签 (2)
15 回复数

2,264 次查看
OtavioSalvador
Senior Contributor II

You most probably need to burn the fuses for use MBR and/or set the boot mode pins accordingly.

0 项奖励

2,264 次查看
RandyGraham
Contributor IV

Thanks Otavio.
We believe we have the boot mode pins set correctly. I'm not sure about the fuses, we are double checking.

2,264 次查看
RandyGraham
Contributor IV

Hmm, everything checks out, voltages, boot mode pins, fuses, but we are still seeing the same boot rom code indicating that it is trying to boot over USB.

We also are not seeing any SPI bus activity for the MMC so it does not seem to be even trying to boot from the SD card.

FWIW, we have another board based on the i.mx28 that we are able to boot from SD with no problems. The same guy designed both boards and he is stumped as to why the i.mx23 board is not booting from SD having checked all the voltages, pin settings, SD card presence switch, etc.

0 项奖励

2,264 次查看
OtavioSalvador
Senior Contributor II

From the Boot ROM error list, it is trying to boot from USB.

#define ERROR_ROM_USB_CONNECT_TIMEOUT (ERROR_ROM_GROUP | ERROR_ROM_USB_DRIVER_GROUP | 0x8)

0x80502008

So it seems it is not falling back to mmc.

0 项奖励

2,264 次查看
RandyGraham
Contributor IV

Yes, it seems so.

0 项奖励

2,264 次查看
OtavioSalvador
Senior Contributor II

I'd do the following; boot the board from USB (using U-Boot) and try to check the MMC from there. If it works, then MMC is fine and it should be a fuse or boot pins issue.   

0 项奖励

2,264 次查看
RandyGraham
Contributor IV

We tried to USB boot u-boot from an SD card plugged into a USB card reader but got the same result.

Can it boot this way ? ie. with a SD card plugged into a USB SD card reader ?

0 项奖励

2,264 次查看
OtavioSalvador
Senior Contributor II

No; you need to boot using a USB loader.

Last time I debugged this kind of issue from a customer board this boosted a lot the test cycle; so I think it is worth setting up the environment.

If your board has the USB_DP and USB_DN pins in the USB connector, it is easy to do.

You can use mxsldr to boot from USB that way. After that, it is a plain U-Boot and you just use it as usual.

0 项奖励

2,264 次查看
RandyGraham
Contributor IV

Ah, yes, of course.

Thanks Octavio, I'll try USB with mxsldr and hopefully get more info on our issue.

Thanks again !!

0 项奖励

2,264 次查看
RandyGraham
Contributor IV

Ok, we found and removed a solder bridge on our board and are now seeing a different rom code.

#define ERROR_DDI_SD_CONFIG_BLOCK_NOT_FOUND (ERROR_DDI_GROUP | ERROR_DDI_SD_DRIVER_GROUP | 0x7)

0x8020A007 ?

Could this mean that that SD card image is bad ?


0 项奖励

2,264 次查看
OtavioSalvador
Senior Contributor II

i.MX23 Reference Manual (page 1372):

HW_OCOTP_ROM0:0x8002C1A0:3

     SD_MBR_BOOT—Set to enable SD Master Boot Record (MBR) mode. The

     SD/MMC card should have a valid MBR to boot successfully in this mode. If this

     bit is not set, ROM will try to boot in default mode, BCB (Boot Control Block).

So our you use BCB or you use MBR ;-)

2,264 次查看
RandyGraham
Contributor IV

Getting closer, thanks Octavio !!

0 项奖励

2,264 次查看
RandyGraham
Contributor IV

Oops, I mean Otavio :smileyhappy:

2,264 次查看
RandyGraham
Contributor IV

I was able to get u-boot running on my board with mxsldr .

What a great tool !

2,264 次查看
RandyGraham
Contributor IV

Talking to our hardware guy, it looks like it might be trying to boot over USB.
I didn't realize that the mx23 ROM supported USB boot.

0 项奖励