We have developed a new PCB starting from mx6sxsabresd design. It currently passes 12h of calibration test without problem,
so the board design should be ok.
The board boot straight with u-boot-imx and it's able to at least boot the first kernel stage until it stops with some printed garbage, the log is below.
It has a custom DTS slight changed from imx6sx-17x17-arm2.dts.
Any idea how to debug it?
Cheers,
Roberto Fichera.
U-Boot 2014.04-imx_v2014.04_3.14.28_1.0.0_ga+g88123ea (Jul 08 2015 - 17:57:57)
CPU: Freescale i.MX6SX rev1.2 at 792 MHz
CPU: Temperature 41 C, calibration data: 0x5ba52269
Reset cause: POR
Board: Domus iMX6SX (ID:e301dab51902b1d4)
I2C: ready
DRAM: 512 MiB
MAX7322 Not found
MMC: FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
Found PFUZE100! deviceid 0x11, revid 0x21
mmc0 is current device
Net: Phy not found
PHY reset timed out
FEC0
Warning: failed to set MAC address
Normal Boot
Hit any key to stop autoboot: 0
=> bdinfo
arch_number = 0x00000000
boot_params = 0x80000100
DRAM bank = 0x00000000
-> start = 0x80000000
-> size = 0x20000000
eth0name = FEC0
ethaddr = (not set)
current eth = FEC0
ip_addr = <NULL>
baudrate = 115200 bps
TLB addr = 0x9FFF0000
relocaddr = 0x9FF66000
reloc off = 0x18766000
irq_sp = 0x9DF63EE0
sp start = 0x9DF63ED0
=> setenv mmcroot /dev/mmcblk3p2 rootwait rw earlyprintk
=> saveenv
Saving Environment to MMC...
Writing to MMC(0)... done
=> boot
mmc0 is current device
mmc0 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
5934672 bytes read in 278 ms (20.4 MiB/s)
Booting from mmc ...
reading domus-reva.dtb
48167 bytes read in 19 ms (2.4 MiB/s)
Kernel image @ 0x80800000 [ 0x000000 - 0x5a8e50 ]
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300ec26
switch to ldo_bypass mode!
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Booting Linux on physical CPU 0x0
Linux version 3.14.28-1.0.0_ga+g91cf351 (roberto@dragon.tekno-soft.it) (gcc version 4.9.2 (GCC) ) #1 SMP PREEMPT Fri Jul 3 12:43:06 CEST 2015
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Voneus i.MX6 SoloX Domus ARM2 Board
bootconsole [earlycon0] enabled
cma: CMA: reserved 320 MiB at 8c000000
Memory policy: Data cache writealloc
PERCPU: Embedded 8 pages/cpu @8bb3a000 s8896 r8192 d15680 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk3p2 rootwait rw earlyprintk
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 176704K/524288K available (7213K kernel code, 394K rwdata, 6196K rodata, 328K init, 428K bss, 347584K reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xa0800000 - 0xff000000 (1512 MB)
lowmem : 0x80000000 - 0xa0000000 ( 512 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x80d20678 (13410 kB)
.init : 0x80d21000 - 0x80d732c0 ( 329 kB)
.data : 0x80d74000 - 0x80dd6ac0 ( 395 kB)
.bss : 0x80dd6acc - 0x80e41d9c ( 429 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32030000, Cache size: 256 kB
*** GARBAGE START HERE ***
Hello,
I have fix the problem for me. What helps me was the kernel commandline parameter initcall_debug. Then I follow the error to the function imx6sx_qos_init in the file arch/arm/mach-imx/mach-imx6sx.c. The error was caused by the statemt writel_relaxed(0, src_base+0x1400); and below. I removed that statements and then then my kernel boots.
Regards
Robert
Hi Roberto
if board based on mx6sxsabresd, why you did not use imx6sx-sdb-reva-ldo.dts ?
Note it is preferably to start with ldo enable option.
Also had you changed ddr settings obtained from
calibration results in uboot/../mx6sx_17x17_arm2/plugin.S
(imx6sx_17x17_ddr3_evk_ddr_setting)
DDR size should be configured in uboot/include/configs/mx6sx_arm2.h,
if you chooses imx6sx-sdb configs then mx6sxsabresd.h.
Additionally one can try to decrease cma size (imx_v7_defconfig
CONFIG_CMA_SIZE_MBYTES=xxx) and use ip=none in kernel boot parameter,
decrease "mem" parameter (refer to attached Release Notes Table 11. Common
kernel boot parameters). Check Table 20. Known issues and workarounds for i.MX 6SoloX
"CSI and LCD cannot be used simultaneously"
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
I did a custom uboot board. We are using 2xDDR3 MT41K128M16JT-125 items, attached you will find the imximage.cfg which I'm not really sure is fine.
Regarding the DTSs I've attached it so you can see the changes, mostly everything is disabled.
In the meantime I will give a try to CONFIG_CMA_SIZE_MBYTES setting.
Hi Roberto
I would suggest to try mx6sxsabresd, imx6sx-sdb-reva-ldo.dts .
~igor
Hi Igor,
already tried the mx6sxsabresd, but doesn't work. Our board is very minimal compared to the mx6sxsabresd and currently we have such pin mapping:
| GROUP | SLIC Signal | Schematic Signal | Board Signal | PAD IOMUX Register | IOMUX Settings | CPU Signal Becomes |
| PCM | PCLK | IMX_PCLK | SD3_DATA1 | IOMUXC_SW_MUX_CTL_PAD_SD3_DATA1 | ALT3 | audmux.AUD6_TXC |
| PCM | FSYNC | FSYNC | SD3_DATA2 | IOMUXC_SW_MUX_CTL_PAD_SD3_DATA2 | ALT3 | audmux.AUD6_TXFS |
| PCM | DTX | SRXD | SD3_DATA0 | IOMUXC_SW_MUX_CTL_PAD_SD3_DATA0 | ALT3 | audmux.AUD6_RXD |
| PCM | DRX | DRX | SD3_DATA3 | IOMUXC_SW_MUX_CTL_PAD_SD3_DATA3 | ALT3 | audmux.AUD6_TXD |
| SPI | SCLK | QSPI1B_SS1_B | QSPI1B_SS1_B | IOMUXC_SW_MUX_CTL_PAD_QSPI1B_SS1_B | ALT3 | ecspi5.SCLK |
| SPI | CS# | QSPI1B_DQS | QSPI1B_DQS | IOMUXC_SW_MUX_CTL_PAD_QSPI1B_DQS | ALT3/ALT5 | ecspi5.SS0/GPIO4_IO28 |
| SPI | SDO | QSPI1A_SS1_B | QSPI1A_SS1_B | IOMUXC_SW_MUX_CTL_PAD_QSPI1A_SS1_B | ALT3 | ecspi5.MISO |
| SPI | SDI | QSPI1A_DQS | QSPI1A_DQS | IOMUXC_SW_MUX_CTL_PAD_QSPI1A_DQS | ALT3 | ecspi5.MOSI |
| Control | RST# | GPIO1_IO11 | GPIO1_IO11 | IOMUXC_SW_MUX_CTL_PAD_GPIO1_IO11 | ALT5 | GPIO1_IO11 |
| Control | INT# | GPIO1_IO12 | GPIO1_IO12 | IOMUXC_SW_MUX_CTL_PAD_GPIO1_IO12 | ALT5 | GPIO1_IO12 |
I've also tried to boot the kernel with CONFIG_CMA_SIZE_MBYTES=32 but doesn't change anything.
Hi Roberto
I would suggest to try *ldo.dts .
For customization support one also can apply to Professional Services
Professional Engineering Services|Freescale
~igor
Hi Roberto
then one can try to run minimal image.
~igor
IMX6_L3.14.28_MFG_TOOL : IMX6_L3.14.28_MFG_TOOL
L3.14.28_1.0.0_iMX6SX_BUNDLE : i.MX 6SoloX Linux Binary Demo Files
also one can try uart_from_osc as kernel boot parameter
~igor
Hi Igor,
I've used fsl-image-gui-x11-imx6sxsabresd.sdcard but still doesn't boot the kernel! See below:
U-Boot 2014.04 (Mar 21 2015 - 01:28:45)
CPU: Freescale i.MX6SX rev1.2 at 792 MHz
CPU: Temperature 44 C, calibration data: 0x5ba52269
Reset cause: POR
Board: MX6SX SABRE SDB
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
Display: Hannstar-XGA (1024x768)
Video: 1024x768x18
gis input --- No input
In: serial
Out: serial
Err: serial
Found PFUZE200! deviceid 0x1, revid 0x21 (?!?!)
mmc0 is current device
Net: Phy not found
PHY reset timed out
FEC0
Warning: failed to set MAC address
Normal Boot
Hit any key to stop autoboot: 0
=> setenv mmcroot /dev/mmcblk1p2 rootwait rw uart_from_osc
=> boot
mmc0 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
5930352 bytes read in 277 ms (20.4 MiB/s)
Booting from mmc ...
reading imx6sx-sdb-reva-ldo.dtb
47064 bytes read in 21 ms (2.1 MiB/s)
Kernel image @ 0x80800000 [ 0x000000 - 0x5a7d70 ]
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300e7d7
Starting kernel ...
.... freeze ....
Hi Roberto
do you have ethernet on board, if not
had you removed FEC driver from linux build ?
~igor
then I think that it is not working, from original U-Boot log:
"
Net: Phy not found
PHY reset timed out
FEC0
Warning: failed to set MAC address"
you shoud set mac address and make it to work so these errors will not appear.
Alternatively one can exclude it temporarily from linux build.
~igor
Hi Igor,
the error come from u-boot-imx. But I've also notice another thing regarding PFUZE!
My uboot wrongly reports
Found PFUZE100! deviceid 0x11, revid 0x21
But the fsl-image-gui-x11-imx6sxsabresd
Found PFUZE200! deviceid 0x1, revid 0x21
Roberto,
I suggest you to set up your own u-boot adapted to your hardware as Igor suggested you above, in case remove all the hw devices not present or not yet configured.
then try to boot your own kernel using the DT suggested again by Igor.
The root filesystem image is irrilevant at this point of the development until you reach the init. but core-image-minimal would be smaller and easier to manage.
Just my 2 cents.
Cordiali Saluti / Kindest Regards / Mit freundlichen Grüßen
--
Marco Cavallini | KOAN sas | Bergamo - Italia
embedded and real-time software engineering
Phone:+39-035-255.235 - Fax:+39-178-22.39.748
Hi Marco,
I've my custom uboot board derived from the mx6sxsabresd because the design started from it. Uboot has been adapted to remove the pinmux conflict against the SLIC wiring. In the DTS I've disabled mostly all the peripherals which are not needed at all.
Hi Roberto
imx6sx-17x17-arm2 board uses pfuse100 while mx6sxsabresd - pfuse200.
In general I would suggest to pay attention to ethernet bring-up and
create new thread for that.
Best regards
igor
Hi Igor,
Regarding pfuse100 vs pfuse200, well it is supposed to be a pfuse200, at least this is what the schematic shown.
I'll cross check with our HW engineer regarding that.
Back to the ethernet bring-up problem, I will open in case a new thread after cross-checking some details with our HW engineer, anyway the item is a LAN8720A.
Cheers,
Roberto Fichera.
Hi Igor,
just had some time to look again to this and I've fixed the MAC problem as well as the PFUSE which now is detected correctly.
U-Boot 2014.04-imx_v2014.04_3.14.28_1.0.0_ga+g88123ea (Aug 28 2015 - 15:38:25)
CPU: Freescale i.MX6SX rev1.2 at 792 MHz
CPU: Temperature 49 C, calibration data: 0x5c553569
Reset cause: POR
Board: Domus iMX6SX (ID:e301dab51823b1d4)
I2C: ready
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
Found PFUZE200! deviceid 0x1, revid 0x21
mmc0 is current device
Net: FEC0
Warning: failed to set MAC address
Normal Boot
Hit any key to stop autoboot: 0
=> bdinfo
arch_number = 0x00000000
boot_params = 0x80000100
DRAM bank = 0x00000000
-> start = 0x80000000
-> size = 0x20000000
eth0name = FEC0
ethaddr = (not set)
current eth = FEC0
ip_addr = <NULL>
baudrate = 115200 bps
TLB addr = 0x9FFF0000
relocaddr = 0x9FF66000
reloc off = 0x18766000
irq_sp = 0x9DF63EE0
sp start = 0x9DF63ED0
=> setenv mmcroot /dev/mmcblk1p2 rootwait rw earlyprintk mem=384M
=> save
Saving Environment to MMC...
Writing to MMC(0)... done
=> boot
mmc0 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
5934680 bytes read in 277 ms (20.4 MiB/s)
Booting from mmc ...
reading domus-reva-ldo.dtb
47642 bytes read in 20 ms (2.3 MiB/s)
Kernel image @ 0x80800000 [ 0x000000 - 0x5a8e58 ]
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300ea19
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Booting Linux on physical CPU 0x0
Linux version 3.14.28-1.0.0_ga+g91cf351 (roberto@dragon.tekno-soft.it) (gcc version 4.9.2 (GCC) ) #1 SMP PREEMPT Fri Aug 28 14:58:41 CEST 2015
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Voneus i.MX6 SoloX Domus Board
bootconsole [earlycon0] enabled
cma: CMA: reserved 32 MiB at 96000000
Memory policy: Data cache writealloc
PERCPU: Embedded 8 pages/cpu @95cca000 s8896 r8192 d15680 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 97536
Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait rw earlyprintk mem=384M
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 342144K/393216K available (7213K kernel code, 394K rwdata, 6196K rodata, 328K init, 428K bss, 51072K reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0x98800000 - 0xff000000 (1640 MB)
lowmem : 0x80000000 - 0x98000000 ( 384 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x80d20678 (13410 kB)
.init : 0x80d21000 - 0x80d732c0 ( 329 kB)
.data : 0x80d74000 - 0x80dd6ac0 ( 395 kB)
.bss : 0x80dd6acc - 0x80e41d9c ( 429 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32030000, Cache size: 256 kB
...then lots of garbage!!!
I've also executed some mtest under uboot:
| DDR3 Device Information | |
| Memory type: | DDR3 |
| Manufacturer: | Micron |
| Memory part number: | MT41K128M16JT-125 |
| Density per chip select (Gb): | 4 |
| Number of Chip Selects per channel used | 1 |
| Total DRAM density (Gb) | 4 |
| Number of ROW Addresses | 14 |
| Number of COLUMN Addresses | 10 |
| Number of BANKS | 8 |
| Bus Width (input 16, 32, or 64 bits) | 32 |
| Clock Cycle Freq (MHz) | 400 |
| Clock Cycle Time (ns) | 2.5 |
Booting this uboot, a straight mtest freeze immediately without an iteration
Normal Boot
Hit any key to stop autoboot: 0
=> mtest
Testing 80000000 ... a0000000:
Pattern 00000000 Writing... <freeze>
Trying to reduce the tested range like below:
Normal Boot
Hit any key to stop autoboot: 0
=> mtest 0x80000000 0x9e000000
Testing 80000000 ... 9e000000:
Pattern 00000000 Writing... Reading...
Mem error @ 0x9DF63D80: found 9FF849E0, expected 077D8F60
Mem error @ 0x9DF63D84: found 9FF8499C, expected 077D8F61
Mem error @ 0x9DF63D88: found 00000000, expected 077D8F62
Mem error @ 0x9DF63D8C: found 9FF7C3E0, expected 077D8F63
Mem error @ 0x9DF63D90: found 9DF63D8C, expected 077D8F64
Mem error @ 0x9DF63D94: found 9FF748B4, expected 077D8F65
Mem error @ 0x9DF63D9C: found 077D8F65, expected 077D8F67
Pattern FFFFFFFF Writing...
reports some errors than freeze, but works with this range:
Hit any key to stop autoboot: 0
=> mtest 0x80000000 0x9d000000
Testing 80000000 ... 9d000000:
Pattern 00000000 Writing... Reading...Iteration: 500
I assume this might depend by the PCB layout below?
TLB addr = 0x9FFF0000
relocaddr = 0x9FF66000
irq_sp = 0x9DF63EE0
sp start = 0x9DF63ED0
Any thought where to look at?
Thanks in advance,
Roberto Fichera.