Custom IMX6Q Hardware Board Bringup Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Custom IMX6Q Hardware Board Bringup Issue

1,010 Views
rajniks
Contributor I

Hello,

I have a custom IMX6Q based hardware. I have checked the power supplies and sequencing of these power supplies and that seems to be okay. I have measured various CAP voltages and they are also fine except VDDUSB_CAP which is 2.7V instead of 3V. Is this a problem?

I have been trying to boot in Serial downloader mode by setting the boot mode pins as required but the Host machine doesn't detect my  board as HID complaint device as explained in DDR Tester User manual.

Can someone suggest some ways in order to make sure that the USB OTG Serial downloader works. Any suggestion is welcome.

Thanks & Regards

Raj Nikumbh

Labels (2)
0 Kudos
Reply
1 Reply

807 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raj

you can try to test processor with SDK (one can run it with jtag)

and test USB interface

i.MX 6Series Platform SDK : Bare-metal SDK

and check all items given in Chapter 2 Design Checklist

Chapter 8 Avoiding Board Bring-up Problems

IMX6DQ6SDLHDG  IMX6DQ6SDLHDG, Hardware Development Guide

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply